SparkFun Forums 

Where electronics enthusiasts find answers.

Questions about the BatchPCB service

Moderator: robacarp

By Batchy
#55222
Working at BatchPCB for a month now, I have seen some common problems. Here are some problems and solutions.

Mirrored Bottom Layers:
Look at your files in a separate gerber file viewer (ie: viewplot) to make sure they look right. You can really notice it when you look at the top and bottom soldermask (aka: stop) and drill layers. If there is a drill hole and only one pad of soldermask, you have mirrored layers.

Centered Gerber Files:
This option was made so you could do your own photo etching. The only problem is that it does not do that for your drill data and it become impossible to accurately realign the drill to gerbers. Once again, using a separate gerber file viewer will help you.

Missing Outline:
It is often better to be explicit about the shape of your board than to leave it up to me or some guy working the routing machine at Gold Phoenix. Check your gerber files in a separate viewer and if you don't see a border, you will get a rectangular board.

DRC Bot:
I understand that a number of people are getting confused by the DRC bot. If you see the warning that says the bot did not recognize your files, don't worry. Scroll down and you can specify which layer belongs to which file. We are working on upgrading our site and the bot uses some legacy code and we are going to upgrade it too. Currently the DRC bot does not check silkscreen or drill files.

Order Status Says: "Customer Attention Needed:"
We have added this status so that if we encounter a problem with your order, you can see it. If you see this, check your email! We wrote an email to you about your order's problem.
By WonkoTheSane
#111862
Do you or any of the staff have any thoughts on why the DRC-bot seems to identify many customers' silkscreen files as soldermask?

My boards come back fine; it's just the DRC bot that seems to mis-identify the silkscreen gerbers.

I posted a question to this effect once (link). Now that the Marketplace is open, I see a lot of people seem to be having this problem. Although, I had seen some boards with all layers properly identified, so I wonder if there's something in my (our) files that the bot is picking up on.

I use pcb version 20070208 on Linux. Looking at my Gerber files, I see every one begins with a comment line like this:
Code: Select all
G04 start of page 2 for group 0 idx 0
This was from the back (solder) side copper layer; the numbers are different for each layer; is it possible the bot is reading this comment and using the page number to assign layers? My version of pcb seems to like these page numbers:

Bottom copper: page 2
Bottom silk: page 8
Bottom mask: page 5
Top copper: page 3
Top silk: page 7
Top mask: page 4

Anyone who gets the right layer assignments from the DRC bot: Do your Gerbers have a comment line like this? Different page numbers?

I'm hardly "fluent" in Gerber; are there any other commands I should look for in the files?

Thanks for any help
By indes
#136882
Take a peek at http://en.wikipedia.org/wiki/G-code#Lis ... d_controls

It states G04 is a dwell code, wait for so many ms without axis movement. I've seen them used in my gerber files similarly to comments, .. I.e.
Code: Select all
G04 Layer_Physical_Order=1*
G04 Layer_Color=255*
It appears they're being used for the editor or CAD application data.

Are you generating RS-247X? or RS-274D?
By hormiguero
#149261
I have done several PCBs on batchpcb before (old site) and had no problems... I tried to submit a PCB design today on the new site - got no email reply from the DRC bot, checking online, it says DRC failed... Looking at the layers, there is no drill view and the filename shows (design name).drl whereas when I uploaded the design, the drill locations were previewed... I tried to re-upload the design under the same name -using edit- after changing the drill file from .TXT to .drl and got nowhere... I also couldn't delete the design... Is there an instruction file for the new website?? New website is pretty, but not functional, lacks info, and doesn't seem to be as intuitive as the old one!!
By colancho
#149289
I'm seeing the same issues as hormiguero - freshly uploaded PCB design shows DRC failed but no DRB bot email nor details as to why.
By lesh11
#149322
Same issue here. After being unable to log in, I created a new user account.

I uploaded a new design. The board failed DRC, but no information why.
This board did pass advanced circuits free dfm.
By badjackson
#149341
same here...i can't delete my old board designs and my new uploaded designs failed the drc, but i never recieved an email to let me know why. ...very frusterating. please post something if anyone finds out how to work around these issues.
By checksix
#149345
I've tried a few tests and none of my submissions ever come out of "drc: submitted" state. And the displayed board dimensions don't match the actual files. For one of my tests I added some random text to the back silkscreen layer and the reported board dimensions changed. And the price dropped to match. Nice.
What a mess. Hope this gets sorted out soon.
By Ziko
#149466
checksix wrote:I've tried a few tests and none of my submissions ever come out of "drc: submitted" state. And the displayed board dimensions don't match the actual files. For one of my tests I added some random text to the back silkscreen layer and the reported board dimensions changed. And the price dropped to match. Nice.
What a mess. Hope this gets sorted out soon.
I also had the same problem. A loaded the first circuit and all is well. The same circuit with some more text has changed size and fails the test drc. No e-mail help me never arrived. I look forward to updates.

P.S. In general, however, a very good job with batchPcb; D
By zkummer
#149904
This new DRC bot is simply terrible...I did some testing and I found that it has no issues with overlapping pins from a different net, yet it has issues with the most simple designs that have nothing wrong with them, other than violating rules that are not listed. For instance, the FAQ says 8 mil traces are accepted, but the same design that works with 9 mil traces fails with 8 mil traces. Plus, the email I get is pretty useless. It has no attachment, and just says, "The drcbot has finished processing your BatchPCB upload #93823. Your board has Failed Visit this page to view or order your board"...to order my failed board???

I'm forced to go thru and submit dozens of test designs to figure out just what this new DRC bot will accept, all because the FAQ has no information on what the new DRC bot is looking for.
By brianrg
#149907
zkummer wrote:This new DRC bot is simply terrible...I did some testing and I found that it has no issues with overlapping pins from a different net, yet it has issues with the most simple designs that have nothing wrong with them, other than violating rules that are not listed. For instance, the FAQ says 8 mil traces are accepted, but the same design that works with 9 mil traces fails with 8 mil traces. Plus, the email I get is pretty useless. It has no attachment, and just says, "The drcbot has finished processing your BatchPCB upload #93823. Your board has Failed Visit this page to view or order your board"...to order my failed board???

I'm forced to go thru and submit dozens of test designs to figure out just what this new DRC bot will accept, all because the FAQ has no information on what the new DRC bot is looking for.
I agree, this sucks! I've ordered several boards about a year ago, now I'm trying to order some more. WTF?
This was such a great service, what happened???
By zkummer
#149968
Did a bit more testing...

-Pin pads can overlap or touch, even if on different nets...so pads that have 0 or negative clearance will pass, but pads with 1-5 mil fail...and 6mil clearance or higher passes.
-Two pin pads on the same net will pass as long as they are not routed...if they are routed, they fail.
-Accepts as little as 1 mil between copper fill and copper/vias.
-8mil traces are not accepted, but 9+ mil are.
-Traces can have any space between them, even touching or overlapping, even when on different nets.
-Will accept a thermal relief line width of 1 (not sure if this is intentional, but it seems wrong given the minimum trace thickness)
-Board outline of 0 or 9 mil is accepted, outlines of 1-8 mil are not.
-Accepts any annular ring width (even 0) for pins and vias.

...I still have a few more items to check, but once I have done them, I am going to make a blank template for FreePCB and post it here.
By zkummer
#150042
If anyone who works for Sparkfun/BatchPCB is reading this, please update the FAQ...this is all that is there:
2 Layer sizing:
8mil (~0.2 mm) spacing minimum
8mil (~0.2 mm) traces minimum
20mil (~0.5 mm) minimum drill size

4 Layer sizing:
6mil (~0.15 mm) spacing minimum
6mil (~0.15 mm) traces minimum
13mil (~0.33 mm) minimum drill size
No blind/buried vias

500mil (~12.7 mm) maximum drill size
-4 layer boards not accepted! Middle layers are shown when editing layers, but board shows as 2-layer after that, and seems to be judged by 2-layer standards.
-6mil and less spacing accepted for almost everything on 2-layer boards.
-Will not accept 8mil traces
-Will accept 1mil and 600mil holes.

So, in spite of the fact that the FAQ only lists a few of the basic design criteria needed to design a reliable board, everything in it is wrong! I've done testing and found the minimums of everything I work with that will be accepted, but I know for a fact that many of the minimums that the DRC accepts are far too low for production, let alone a reliable circuit.

PLEASE...if anyone with the specs from the manufacturer is reading this, update the FAQ with the following (or at least post it here):

Minimum pad to pad clearance
Minimum pad to trace clearance
Minimum trace to trace clearance
Minimum hole to pad clearance
Minimum hole to trace clearance
Minimum copper to copper fill clearance
Minimum hole-edge to copper fill clearance
Minimum thermal relief line width
Minimum annular ring width for pads
Minimum annular ring width for vias
Minimum & maximum hole sizes
Minimum via hole size
Minimum distance from board edge to any copper
Minimum distance between copper areas
Minimum trace width (if it is 8, please set the DRC to use a float slightly below 8 so they are not rejected)
By zkummer
#150043
Here is the blank template for new BatchPCB DRC Bot, I made some educated guesses as to what is actually safe for some things, as DRC bot accepts things that are clearly unsafe. This might waste a little bit of board space, but at least the circuits should work. There are some things I cannot put in a template, such as minimum pin size...so a little bit of logic is still required when designing boards. Also, if you want to run a copper area to the edge of the board, the DRC will accept it, but the FreePCB DRC will reject it with this template...in this specific situation, just ignore the errors relating to the copper areas; it will still make gerber files.
You do not have the required permissions to view the files attached to this post.
By BigMc
#151053
Much thanks to zkummer and others who contributed. After fighting DRC for a couple of hours I turned to the forums. I noted the exceptions to the DRC checker you outlined, made a couple of very minor fixes and bingo! DRC is now happy. For me all I had to do was change the board outline from 8mil to 9mil since the board was designed with 10/10 rules. I did download your template but cannot import it into my CAD tool set and honestly would rather not download and install FreePCB if I don't have to. Could I please request you post a written list. Could be text in a reply or txt/csv/??? or other common format. Would be exceptionly helpful and if in a .txt could be edited/added to/etc by others and reposted as a repository that could easily be downloaded but just a written reply would be good too. Thanks again for you efforts to corner this beast as I know all to well how much time you must have put into getting this information. You absolutely saved me lots of hours.

Now the problem is that it thinks my board is 1sq inch when in fact it's 4.8 sq inches. I'll continue to read the forums for hints but is seems to me that if they are not going to use lines around the outside (this one is a rectangle) they should put something in the FAQ that tells us how to establish the board outline. I did read everything on the site I could which is why I drew the outline on every layer but no cigar.

Mike