PCB CNC machine

Questions about the BatchPCB service

Moderators: phalanx, robacarp

Re: PCB CNC machine

Postby rf333 » Sat Oct 12, 2013 11:37 am

Hi @marianmp,
The maximum depth setting that the SW allows me is 11.4 mm , but this is actually the entire travel of the pressure foot (looking at the reading of the gauge). I definitely believe that machining depth of any kind up to 11 mm is not a problem. In your particular case the aspect ratio is quite impressive 9.5/0.68 and definitely will require the use of peck mode. In my model it is completely automated, but still adds up to the machining time.
On the other hand it is impossible to do this ratio with standard single pass drilling. You definitely will break the tool on the first hole.
You better contact accuratecnc for more details.
I notice that they have bunch of new models... and mine is already an old one :(
rf333
 
Posts: 26
Joined: Tue Feb 24, 2009 10:20 am

Re: PCB CNC machine

Postby marianmp » Tue Nov 26, 2013 6:45 am

Hello @rf333,
Thank you for the help. Finally I ordered the top model http://www.accuratecnc.com/Specs/A637.pdf with vaccum table and expect to receive it for Christmas :)
marianmp
 
Posts: 6
Joined: Tue Mar 03, 2009 11:25 pm

Previous

Return to BatchPCB

Who is online

Users browsing this forum: No registered users and 4 guests