SparkFun Forums 

Where electronics enthusiasts find answers.

General suggestions or questions about the SparkFun Electronics website
By Bob_Yeatman
#162963
Hi,
I have a sensor that gives my yaw, pitch and roll. How do I convert these values into azimuth and elevation (tilt). I have seen web pages giving lots of matrix match stuff. Can someone give me an example procedure/function (basic, C, Delphi, etc) that accepts the yaw, pitch and roll values and returns the azimuth and elevation (tilt). Any help would be appreciated!
Bob
By Valen
#162976
Isn't yaw equivalent to azimuth, and pitch equivalent to elevation/tilt? Roll is a rotation along the resulting axis, so won't influence azimuth or elevation. Or is there an angular offset between these axis systems. What sort of thing are you darting around in the air here?
By Bob_Yeatman
#163153
This sensor in inside of a long thin probe that goes into a borehole (no darting around in the air). The probe is often in a near vertical position but can also be used in a borehole tilted up to about 45 degrees. My problem is this... in a near vertical position turning the probe along its longitudinal axis changes the sensor's azimuth value (its how a point on the side of the probe is oriented relative to north - the compass); the roll and pitch are both about 0 because the probe is about vertical. When the probe is tilted at a 45 degree angle it seems to me that the roll and pitch now define the orientation of the probe's longitudinal axis (for example the probe's longitudinal axis is pointing north). The original azimuth value is now the probe's roll in the borehole. Very confusing :-) Do you have any idea where I can find functions that will give me the probe's azimuth (compass direction of the probe's longitudinal axis) and elevation in an inclined borehole? Would these functions work when the probe in in a near vertical position? Thanks!
By Mee_n_Mac
#163156
I think you will need to supply a link to the probe/sensor so "we" can see how the manufacturer defines the sensor's axes. Otherwise the definition of X, Y and Z, pitch, yaw and roll, etc will become very confused. My natural tendency is to think that rotation about the longitudinal axis would be called roll, yet you say the sensor changes it's Az value.