Bluetooth modem bluesmirf silver

General suggestions or questions about the SparkFun Electronics website

Moderators: phalanx, CS Paul

Post Reply
ebourlas
Posts: 1
Joined: Fri Mar 01, 2013 11:07 am

Bluetooth modem bluesmirf silver

Post by ebourlas » Fri Mar 01, 2013 11:17 am

I have recently purchased the Bluetooth Modem Bluesmirf Silver breakout board and had some questions about the design. What is the purpose of the BSS138 N-Channel Logic Level Enhancement Mode Field Effect Transistors, and are they necessary when designing a surface mount with an ATMEGA328 with 3.3V input?

User avatar
SFE-Toni
SFE Guru
Posts: 121
Joined: Thu Nov 15, 2012 12:13 pm
Location: Boulder, CO, USA

Re: Bluetooth modem bluesmirf silver

Post by SFE-Toni » Fri Mar 01, 2013 4:21 pm

The transistors are included to shift logic levels from a 5v system to the 3.3v that the RN-42 module communicates at. If you will be hooking up the module to a 3.3v system, then you do not need to include these into your system. We designed the BlueSMirF and Bluetooth Mate boards to be able to interface with 3.3v-6v systems to make them more user-friendly for our customers.

Post Reply