advice for max44000?

General suggestions or questions about the SparkFun Electronics website

Moderators: phalanx, CS Paul

Post Reply
8Volts
Posts: 114
Joined: Mon Nov 22, 2010 8:01 pm

advice for max44000?

Post by 8Volts » Sun Feb 17, 2013 9:19 am

hello,

I have achieved a proximity sensor circuit with
the tsop4838 ir sensor. However, I just ran into this part:

http://catalog.gaw.ru/project/download.php?id=39995

Now, I would like to know if anyone used the max44000
part for proximity sensing ????

And can anyone tell me what is the maximum distance
that the max44000 part can detect an object. In the spec
it says 1.5 uw/cms LSB??? From that info, how can one deduct it's
maximum proximity capability???

http://mobile.findchips.com/avail?part=max4400

Also, what would be the benefits of using
the tsop solution versus the max44000 solution.

It seems to me that the max44000 is much simpler
to connect given that it takes care of all the
signal bursts for you!!!

a little undecided,I would really need another
point of view!!!

All feedback is sincerely appreciated!
r
Last edited by 8Volts on Mon Feb 18, 2013 7:48 pm, edited 1 time in total.

CS Paul
Posts: 128
Joined: Fri Apr 02, 2010 7:37 am

Re: advice for max44000?

Post by CS Paul » Mon Feb 18, 2013 8:14 am

I don't have an answer for you, but you'll probably find more help over in the technical side of the forums. The folks who can actually help help probably won't see your post here.

8Volts
Posts: 114
Joined: Mon Nov 22, 2010 8:01 pm

Re: advice for max44000?

Post by 8Volts » Mon Feb 18, 2013 7:51 pm

Thanks CS Paul....

I don't think I am going to switch... as the costs
are very comparable between what I am doing
and what the max44000 is doing given that they too
have to use extra hardware if they want to have
a greater detection range than 30cm!

thanks for replying!

r

Post Reply