"silly" noob question

General suggestions or questions about the SparkFun Electronics website

Moderators: phalanx, CS Paul

Post Reply
Beanbag109
Posts: 2
Joined: Thu Feb 09, 2012 12:41 pm

"silly" noob question

Post by Beanbag109 » Thu Feb 09, 2012 4:56 pm

Could someone help a noob?

Could someone please tell me what a "breakout" board is in VERY basic terms. I am soooo new to all of this.

Thanks
Mike

User avatar
leon_heller
Support Volunteer
Posts: 5734
Joined: Sun May 01, 2005 11:20 am
Location: St. Leonards-on-Sea, E. Sussex, UK.

Re: "silly" noob question

Post by leon_heller » Thu Feb 09, 2012 8:25 pm

It''s a PCB for a fine pitch device that brings the leads out to wider pads, making it easy to wire it into a circuit.
Leon Heller
G1HSM

Beanbag109
Posts: 2
Joined: Thu Feb 09, 2012 12:41 pm

Re: "silly" noob question

Post by Beanbag109 » Fri Feb 10, 2012 11:22 pm

okay, so, (knowledge check) it is a board that will attach to a "main" board, that does a certin task, that is larger-and easy to work on.
A) True
B) False

C) All of the above... lol, just kidding

Thanks for the help!
Mike

CS Paul
Posts: 128
Joined: Fri Apr 02, 2010 7:37 am

Re: "silly" noob question

Post by CS Paul » Mon Feb 13, 2012 10:52 am

D) Not sure what you mean

Things in this category are breakout boards:

http://www.sparkfun.com/categories/20

n1ist
Support Volunteer
Posts: 1009
Joined: Wed Mar 22, 2006 11:02 am

Re: "silly" noob question

Post by n1ist » Tue Feb 14, 2012 8:59 am

To combine all the above: Breakout boards often describe one of two things

- Adapters to convert either connectors or ICs to a convenient footprint. This includes ones that go from a fine-pitch LCD connector to 0.1" headers, and boards with hard-to-mount parts (tiny surface mount parts, BGA or QFN footprints) and a header or connector. They often include other components that are always needed or have to be close to the part (bypass caps, pullup resistors, crystals). http://www.sparkfun.com/products/9614 and http://www.sparkfun.com/products/9719 are examples of this type

- Modules that encapsulate functionality, like a complete MP3 decoder/audio amp or USB to serial interface, that can be used as part of a larger project. http://www.sparkfun.com/products/10277 and http://www.sparkfun.com/products/718 are examples of this type

/mike

Post Reply