hello its good. Can you provide me code of v2xe. As your data show that you had completed it. i am university student and doing project. i shall be very thankful to you if you provide me that code and the one i wrote kindly check it out.
Code: Select all/*
V2XE code based on:
V2XE Example.c
Created by John Gonzaga on Thu Dec 18 2003.
Copyright (c) 2003 PNI Corporation. All rights reserved.
SPI code based on:
Spi.cpp - SPI library
Copyright (c) 2008 Cam Thompson.
Author: Cam Thompson, Micromega Corporation, <www.micromegacorp.com>
Version: December 15, 2008
*/
#include<SPI.h>
#define SCK_PIN 13
#define MISO_PIN 12
#define MOSI_PIN 11
#define SYNC_PIN 10
const int chipSelectPin = 7;
#define kSyncChar 0xAA
#define kTerminator 0x00
enum
{
// commands/frame types
kGetModInfo = 1, // 0x01
kModInfoResp, // 0x02
kSetDataComponents, // 0x03
kGetData, // 0x04
kDataResp, // 0x05
kSetConfig, // 0x06
kGetConfig, // 0x07
kConfigResp, // 0x08
kSaveConfig, // 0x09
kStartCal, // 0x0A
kStopCal, // 0x0B
kGetCalData, // 0x0C
kCalDataResp, // 0x0D
kSetCalData, // 0x0E
// data types
kRawX = 1, // 0x01
kRawY, // 0x02
kCalibratedX, // 0x03
kCalibratedY, // 0x04
kHeading, // 0x05
kMagnitude, // 0x06
kTemperature, // 0x07
kDistortion, // 0x08
kCalStatus, // 0x09
// config types
kDeclination = 1, // 0x01
kTrueNorth, // 0x02
kCalSampleFreq, // 0x03
kSampleFreq, // 0x04
kPeriod, // 0x05
kBigEndian, // 0x06
kDampingSize, // 0x07
// cal data types
kXOffset = 1, // 0x01
kYOffset, // 0x02
kXGain, // 0x03
kYGain, // 0x04
kPhi, // 0x05
kCalMagnitude // 0x06
};
/* TODO clean this up*/
typedef struct
{
long x, y;
float xe, ye;
float heading, magnitude;
float temperature;
byte distortion, calStatus;
} V2XEData;
V2XEData* data;
void init_compass(){
byte tmp;
// initialize the SPI pins
pinMode(SCK_PIN, OUTPUT);
pinMode(MOSI_PIN, OUTPUT);
pinMode(MISO_PIN, INPUT);
pinMode(chipSelectPin, OUTPUT);
pinMode(SYNC_PIN, OUTPUT);
digitalWrite(SYNC_PIN, LOW);
// The V2Xe must be talked to at f <= 3.6864 MHz -> FOSC/4
// enable SPI Master, MSB, SPI mode 0, FOSC/4 (= 2MHz on the 3,3v, 8MHz arduino mini pro)
//mode(2);
delay(20);
// sync the compass
v2xe_sync();
}
void mode(byte config){
// have a look at the atmega datasheet for meaning of the config parameter.
byte tmp;
// enable SPI master with configuration byte specified
SPCR = 0;
SPCR = (config & 0x7F) | (1<<SPE) | (1<<MSTR);
tmp = SPSR;
tmp = SPDR;
}
void v2xe_sync(){
digitalWrite(SYNC_PIN, LOW);
delayMicroseconds(100);
digitalWrite(SYNC_PIN, HIGH);
delayMicroseconds(100);
digitalWrite(SYNC_PIN, LOW);
delay(20);
}
// low level transmission function
byte spi_transmit(byte value){
SPDR = value;
while (!(SPSR & (1<<SPIF))) ;
return SPDR;
}
//Higher level transmission functions
//----------------------------------------
byte spi_receive_byte(){
return spi_transmit(0);
}
//Endinaness s by default the "wrong one" (aka not he one used by the arduino)
unsigned long spi_receive_ulong(){
unsigned long res = ((unsigned long)spi_transmit(0)) << 24
| ((unsigned long)spi_transmit(0)) << 16
| ((unsigned long)spi_transmit(0)) << 8
| ((unsigned long)spi_transmit(0)) ;
return res;
}
/*
// TODO revert the endianess of the compass and use this function instead
unsigned long spi_receive_ulong(){
unsigned long res = ((unsigned long)spi_transmit(0))
| ((unsigned long)spi_transmit(0)) << 8
| ((unsigned long)spi_transmit(0)) << 16
| ((unsigned long)spi_transmit(0)) << 24;
return res;
}*/
long spi_receive_long(){
unsigned long res = spi_receive_ulong();
return *((long*)((void*)&res));
}
float spi_receive_float(){
unsigned long res = spi_receive_ulong();
return *((float*)((void*)&res));
}
void ask_mod_info(){
byte index, count, type, buffer[64];
index = 0;
buffer[index++] = kSyncChar; // all frames always start with a sync character
buffer[index++] = kGetModInfo; // the frame type
buffer[index++] = kTerminator; // don't forget the terminator
// now transmit the command
count = index;
index = 0;
while(count--){
// just throw away whatever is receive
spi_transmit(buffer[index++]);
}
}
void ask_heading(){
byte index, count, type, buffer[64];
index = 0;
buffer[index++] = kSyncChar; // all frames always start with a sync character
buffer[index++] = kSetDataComponents; // the frame type
buffer[index++] = 1; // number of components to retrieve
buffer[index++] = kHeading;
buffer[index++] = kTerminator; // don't forget the terminator
// now transmit the command
count = index;
index = 0;
while(count--){
// just throw away whatever is receive
spi_transmit(buffer[index++]);
}
}
void get_data(){
byte index, count, type, buffer[64];
index = 0;
buffer[index++] = kSyncChar; // all frames always start with a sync character
buffer[index++] = kGetData; // the frame type
buffer[index++] = kTerminator; // don't forget the terminator
// now transmit the command
count = index;
index = 0;
while(count--){
// just throw away whatever is receive
spi_transmit(buffer[index++]);
}
}
void receive_data(){
byte frame, count, type;
// now poll the response by looking for the response SyncChar
while(spi_receive_byte() != kSyncChar) delayMicroseconds(250);
frame = spi_receive_byte();
// the next byte will be the response frame type
if(frame == kDataResp){
// the next byte will be the data component count
count = spi_receive_byte();
while(count--){
// get the component data identifier
type = spi_receive_byte();
switch(type){
case kRawX:
data->x = spi_receive_long();
// The "long" raw X count is now stored in data->x
// The V2Xe can return in little endian or big endian
// format, so prior to any transmission set the
// V2Xe endian format
break;
case kRawY:
data->y = spi_receive_long();
break;
case kCalibratedX:
data->xe = spi_receive_float();
break;
case kCalibratedY:
data->ye = spi_receive_float();
break;
case kHeading:
data->heading = spi_receive_float();
break;
case kMagnitude:
data->magnitude = spi_receive_float();
break;
case kTemperature:
data->temperature = spi_receive_float();
break;
case kDistortion:
data->distortion = spi_receive_byte();
break;
case kCalStatus:
data->calStatus = spi_receive_byte();
break;
default:
// error condition
break;
}
}
}
Serial.println((int) data->heading );
// cleanup of the eventual garbage
while(spi_receive_byte() != kTerminator);
}
void GetData()
{
byte index, count, type, buffer[64];
index = 0;
// send SetDataComponents command to get all the data
// the order of the components
buffer[index++] = kSyncChar; // all frames always start with a sync character
buffer[index++] = kSetDataComponents; // the frame type
buffer[index++] = 9; // number of components to retrieve
buffer[index++] = kRawX; // followed by the component identifiers
buffer[index++] = kRawY; // ... the order of the identifiers
buffer[index++] = kCalibratedX; // ... will the same in the response
buffer[index++] = kCalibratedY; // ... frame, DataResp
buffer[index++] = kHeading;
buffer[index++] = kMagnitude;
buffer[index++] = kTemperature;
buffer[index++] = kDistortion;
buffer[index++] = kCalStatus;
buffer[index++] = kTerminator; // don't forget the terminator
// now transmit the command
count = index;
index = 0;
while(count--)
{
// just throw away whatever is receive
spi_transmit(buffer[index++]);
}
// now poll the response by looking for the response SyncChar
while(spi_receive_byte() == kSyncChar);
// the next byte will be the response frame type
if(spi_receive_byte() == kDataResp)
{
// the next byte will be the data component count
count = spi_receive_byte();
while(count--)
{
// get the component data identifier
type = (0);
switch(type)
{
case kRawX:
data->x = spi_receive_long();
// The "long" raw X count is now stored in data->x
// The V2Xe can return in little endian or big endian
// format, so prior to any transmission set the
// V2Xe endian format
break;
case kRawY:
data->y = spi_receive_long();
break;
case kCalibratedX:
data->xe = spi_receive_float();
break;
case kCalibratedY:
data->ye = spi_receive_float();
break;
case kHeading:
data->heading = spi_receive_float();
break;
case kMagnitude:
data->magnitude = spi_receive_float();
break;
case kTemperature:
data->temperature = spi_receive_float();
break;
case kDistortion:
data->distortion = spi_receive_byte();
break;
case kCalStatus:
data->calStatus = spi_receive_byte();
break;
default:
// error condition
break;
}
}
}
}
void setup()
{
Serial.begin(9600);
SPI.setClockDivider(SPI_CLOCK_DIV8);
SPI.begin();
SPI.setDataMode(SPI_MODE0);
}
void loop()
{
digitalWrite(chipSelectPin, LOW);
GetData();
Serial.println(data->heading);
digitalWrite(chipSelectPin, HIGH);
}