- Wed May 22, 2019 9:11 am
#204468
I recently purchased some of the SparkFun MLX90640 breakout boards, but of the 5 I have, only 2 are working. The other three I can connect to the same microcontroller and program (as described in the Hookup Guide [https://learn.sparkfun.com/tutorials/qw ... -guide/all]), but they all have the same error of "Parameter extraction failed." The pixels only read "nan" instead of temperature value.
Is there something that I can adjust on the sensors/in the program to allow these sensors to work, or should I just return them? Once again, two of the sensors (one V10 and one V12) work fine, but the other three (all V12's) have the above error when connected to the same MCU and program as the first two.
Is there something that I can adjust on the sensors/in the program to allow these sensors to work, or should I just return them? Once again, two of the sensors (one V10 and one V12) work fine, but the other three (all V12's) have the above error when connected to the same MCU and program as the first two.