Code: Select allThat's because you aren't cleaning the copper well enough. Use a fine scotch brite pad, then wipe with acetone until you don't see any residue. Also be careful when you handle the PnP, not to get your acid and oil covered fingers on the toner surface.
Of the 5 or 6 times ive tried it now, 1 time I used 600 grit sandpaper with a jitterbug sander. The copper literally had a mirror finish when i was done. I used regular tap water to clean the dust and stuff off, not acetone... maybe thats a problem? All other times i just used a brillo pad and scrubed the hell outa it. But again just used tap water to clean it. Always handled them on the edges, never got prints on them.
Is the toner not transferring at all, or is it just not transferring cleanly?
I use the other brand too, but I'd expect the PnP stuff to work just as well. With the stuff I use, the only things I can think of that would completely prevent transfer are: not using a laser printer/copier, not having the iron hot enough, or printing on the wrong side of the paper.
Eh, my best attempt was today and i guess it was pretty good. It was just some random thing i printed out because i have given up on any real circuit (for now) and am just focusing on getting something at least. If it had been a real circuit it defiantly wouldn't had worked without major rework and solder spots etc.
Im trying to find a good middle ground with the iron still. THe wool setting docent seem to be hot enough like the directions call for and sometimes i set it too high and the PNP just ends up shriveling.
If you're getting partial transfer, you can try cleaning the board better, changing the iron's heat setting or ironing time, altering the amount of pressure when ironing, or moving the iron around. Also, crank up the darkness setting on your printer, shake the toner cartridge a little before printing, and if your printer has very good alignment you could run it through the printer twice to increase the amount of toner deposited.
a lota the times i put almost my full weight on the iron. i have the printer set to 600DPI
Ill have another go at it tomorrow. I had really given up after my last failed attempt today but your suggestions have given me a 2nd wind. Ill try some of stuff you guys said. Thank you!