- Mon Nov 06, 2006 4:58 pm
#21478
I am trying to interface a DOSonCHIP to the RS232 level shifter. I am powering the device and the level shifter at 3.7VDC from an Li+ and I am able to get the level shifter TX LED to flicker when i type. However, I am unable to obtain any response from the device.
I have VCC and GND connected up, as well as TX and RX on the UART interface lines tied to the level shifter. the MODE's are floating as it says to do this if its in UART mode. I noticed that there are some hardware flow control lines on the device.
I have tried to directly interface the hardware flow control lines directly to my PC's serial interface as they are "5VDC tolerant", but it does not seem to work.
I suspect that either the module is defective, or perhaps the 3VDC level for the hardware handshake is too low for it to send the data from the DOSonCHIP to my PC.
Any ideas?
I have VCC and GND connected up, as well as TX and RX on the UART interface lines tied to the level shifter. the MODE's are floating as it says to do this if its in UART mode. I noticed that there are some hardware flow control lines on the device.
I have tried to directly interface the hardware flow control lines directly to my PC's serial interface as they are "5VDC tolerant", but it does not seem to work.
I suspect that either the module is defective, or perhaps the 3VDC level for the hardware handshake is too low for it to send the data from the DOSonCHIP to my PC.
Any ideas?