Sparkfun USB Host Controller

Have questions about a SparkFun product or board? This is the place to be.

Moderator: phalanx

Post Reply
hbear2015108
Posts: 2
Joined: Mon Jan 15, 2018 10:28 am

Sparkfun USB Host Controller

Post by hbear2015108 » Sun Jan 20, 2019 5:17 pm

Hi,
I have a USB Shield DEV-09947 and am using scripts from the examples provided with the library: USB_Host_Shield_2.0-master in conjunction with an Arduino R3 UNO. Right now, I am working with the script hub_demo, though the same issue has arisen with an example script with a mouse and a joystick.
In all cases, when I press the reset button on the board or not after uploading, I get the following in the serial window:

Start
OSC did not start

That's it. Any suggestions?

Post Reply