SparkFun Forums 

Where electronics enthusiasts find answers.

Have questions about a SparkFun product or board? This is the place to be.
By BigPilot
#201321
I noticed that most projects using the Si470x tuner breakout are using 3.3V to drive the board. However, in the Si4702 datasheet I noticed that it can be powered by 5V. Is it safe to use it with a 5V microcontroller such as the Teensy 2.0 (AVR) I'm using?
By BigPilot
#201334
Also, the schematic says: '2.7V < VCC < 3.3V', implying that the board cannot be powered by 5V.
By BLH
#201336
I would say no.
Look at the data sheet again. VD and VA can be 5 volts. The VIO voltage is rated 1.5 to 3.6 volts.
The schematic shows VD,VA and VIO are all on one voltage input connection.
By BigPilot
#201338
Yeah, you're right. VIO has an absolute maximum rating of 3.9V.

Luckily, I still have a couple of Sparkfun level converters lying around. ;)
long long title how many chars? lets see 123 ok more? yes 60

We have created lots of YouTube videos just so you can achieve [...]

Another post test yes yes yes or no, maybe ni? :-/

The best flat phpBB theme around. Period. Fine craftmanship and [...]

Do you need a super MOD? Well here it is. chew on this

All you need is right here. Content tag, SEO, listing, Pizza and spaghetti [...]

Lasagna on me this time ok? I got plenty of cash

this should be fantastic. but what about links,images, bbcodes etc etc? [...]