SparkFun Forums 

Where electronics enthusiasts find answers.

Have questions about a SparkFun product or board? This is the place to be.
By jxmot-iot
#200093
Hello,

I'd like to use the BOB-12009(https://www.sparkfun.com/products/12009) or something similar to drive a DHT22 module that's powered with 5v. And communicating with ESP-01 @ ~3.3v. Will this device work for communicating with the DHT22?

Also, what is the maximum voltage difference between LV and HV for this device?

Thanks in advance!
By paulvha
#200097
This could be used turn the ouput signal (max 5V) from the DHT22 to the ESP (max 3V3). As it only one data line, you could also make a voltage divider with 2 resistors or you can use the DHT22 on 3v3,

The HV looks to be max 50V and the LV ~20V ( but this based on the used BSS138 data sheet)