- Sun Aug 12, 2018 12:30 pm
#200032
I'm having no success with Example1_Constant_Read for the Simultaneous RFID Reader. I first changed line 277 in the library implementation file from:
When running the example, the sketch stops at line 28, when the setupNano() call returns false, printing "Module failed to respond. Please check wiring." I'm not using it as a shield, I've just bread-boarded pin 2 on the reader to pin 2 on an Uno and pin 3 to pin 3 on the Uno (I also tried the reverse). The switch on the reader is in SW_UART. The reader is being powered by a 5V wall-wart and does work over USB with the UniversalReaderAssistant program.
Can someone point out what is missing in my setup?
Code: Select all
to
return (writeData(bank, address, newID, newIDLength, timeOut));
Code: Select all
...because the compiler threw an error on the implicit cast. The example sketch hasn't been changed though.return (writeData(bank, address, (uint8_t*)newID, newIDLength, timeOut));
When running the example, the sketch stops at line 28, when the setupNano() call returns false, printing "Module failed to respond. Please check wiring." I'm not using it as a shield, I've just bread-boarded pin 2 on the reader to pin 2 on an Uno and pin 3 to pin 3 on the Uno (I also tried the reverse). The switch on the reader is in SW_UART. The reader is being powered by a 5V wall-wart and does work over USB with the UniversalReaderAssistant program.
Can someone point out what is missing in my setup?