cannot config "active low" interrupt for lsm303c

Have questions about a SparkFun product or board? This is the place to be.

Moderator: phalanx

Post Reply
gilo12
Posts: 1
Joined: Tue Jul 31, 2018 4:12 am

cannot config "active low" interrupt for lsm303c

Post by gilo12 » Tue Jul 31, 2018 4:41 am

Hi all,

I am activating a SparkFun 6 Degrees of Freedom Breakout - LSM303C with pic18f86j90. My goal is to get an acceleration interrupt on XYZ axis, then go and read the magnetometer position and make some descision upon it.

But, i am not able to get the INT_XL pin working on "active low".

The lsm303c INT_XL pin is configured as "active low" and "open-drain". see code below.

I have configured the pic18 port as input with weak pull-up. The breakout board does react to accreleration, but works the opposite way: normally signal is low and when interrupt happenns, INT_XL goes high for about 40ms and then comes back to low.

The accelerometer initialization routine is:
void LSM303C_AccInit(void)
{
uint8_t result = 0;

output_high(PIN_F3);
ACCELERO_IO_Write(LSM303C_CTRL_REG1_A, 0b00100101); // disable y axis to avoid mg

ACCELERO_IO_Write(LSM303C_CTRL_REG2_A, 0b00000000);

ACCELERO_IO_Write(LSM303C_CTRL_REG3_A, 0b00001000); //was 1101

ACCELERO_IO_Write(LSM303C_CTRL_REG4_A, 0b00000000);


ACCELERO_IO_Write(LSM303C_CTRL_REG5_A, 0b00000011); //interrupt active low, open-drain


/// ACCELERO_IO_Write(LSM303C_CTRL_REG7_A, 0b00000100); //1: interrupt request latched Cleared by reading IG_SRC[2:1]_A register


ACCELERO_IO_Write(LSM303C_FIFO_CTRL, 0b01000000); //stream mode,

ACCELERO_IO_Write(LSM303C_IG_CFG1_A, 0b11100010); //y interrupt disabled

ACCELERO_IO_Write(LSM303C_IG_THS_X1_A, 5);
ACCELERO_IO_Write(LSM303C_IG_THS_Y1_A, 5);
ACCELERO_IO_Write(LSM303C_IG_THS_Z1_A, 5);

ACCELERO_IO_Write(LSM303C_IG_DUR1_A, 0b10000001); //interrupt delay


}

Can you please let me know what is wrong with my config?

Thanks,

Gil

Post Reply