Using WAV Trigger as a 16PAS sample launcher

Have questions about a SparkFun product or board? This is the place to be.

Moderator: phalanx

Post Reply
Element103
Posts: 1
Joined: Thu May 03, 2018 5:07 am

Using WAV Trigger as a 16PAS sample launcher

Post by Element103 » Thu May 03, 2018 5:41 am

Hi everyone,
Yesterday I discovered this WAV Trigger board and I fell in love with it, but I need some infos!

I want to use it as an MPC or StandAlone sample player to jam and to make some hip hop beats (sketched up a design on solidworks https://imgur.com/a/dpGlC64 ).
The thing that makes me think is that the board itself has 16 inputs, meaning that if I want a button or anything to trigger the "change bank" command I'll have to sacrifice 2 inputs in order scroll up and down into the folders (as shown in the sketch I made).
I saw that the board can get inputs from the digital outputs of board such as Arduino (I have a UNO and a NANO laying around in my bedroom) and I thought that this way I can have all the 16 triggers for the arcade buttons.
I'm a complete noob in programming Arduino, so I can't modify existing codes...

Can someone help me? Is it possible to do this?

Post Reply