- Thu Feb 08, 2018 6:31 am
#198244
Hello, I recently purchased a Tiny AVR programmer from sparkfun.
I also got a ATtiny 85 from mouser.
https://www.mouser.com/ProductDetail/Mi ... bkrw%3d%3d
I correctly followed the hookup guide.
Since I have WIndows 8.1, I disabled the driver signiture. Please note, that when I rebooted for the last time, the computer didn't ask me anything.
I ran a simple program, the 1st one listed here:
https://learn.sparkfun.com/tutorials/ti ... gKRYvD_BwE
And I got this error:
Any help would be appreciated.
Thank You.
I also got a ATtiny 85 from mouser.
https://www.mouser.com/ProductDetail/Mi ... bkrw%3d%3d
I correctly followed the hookup guide.
Since I have WIndows 8.1, I disabled the driver signiture. Please note, that when I rebooted for the last time, the computer didn't ask me anything.
I ran a simple program, the 1st one listed here:
https://learn.sparkfun.com/tutorials/ti ... gKRYvD_BwE
And I got this error:
Code: Select all
Arduino: 1.8.5 (Windows 8.1), Board: "ATtiny, ATtiny85, 1 MHz (internal)"
Archiving built core (caching) in: C:\Users\user\AppData\Local\Temp\arduino_cache_189879\core\core_attiny_avr_attiny_cpu_attiny85,clock_internal1_b66a9c5c76b69370244e620b5a0a7ae0.a
Sketch uses 686 bytes (8%) of program storage space. Maximum is 8192 bytes.
Global variables use 9 bytes of dynamic memory.
C:\Users\user\AppData\Local\Arduino15\packages\arduino\tools\avrdude\6.3.0-arduino9/bin/avrdude -CC:\Users\user\AppData\Local\Arduino15\packages\arduino\tools\avrdude\6.3.0-arduino9/etc/avrdude.conf -v -pattiny85 -cusbtiny -Uflash:w:C:\Users\user\AppData\Local\Temp\arduino_build_418884/ATtiny85test.ino.hex:i
avrdude: Version 6.3, compiled on Jan 17 2017 at 12:00:53
Copyright (c) 2000-2005 Brian Dean, http://www.bdmicro.com/
Copyright (c) 2007-2014 Joerg Wunsch
System wide configuration file is "C:\Users\user\AppData\Local\Arduino15\packages\arduino\tools\avrdude\6.3.0-arduino9/etc/avrdude.conf"
An error occurred while uploading the sketch
Using Port : usb
Using Programmer : usbtiny
avrdude: Error: Could not find USBtiny device (0x1781/0xc9f)
avrdude done. Thank you.
This report would have more information with
"Show verbose output during compilation"
option enabled in File -> Preferences.
Any help would be appreciated.
Thank You.