- Mon Feb 05, 2018 6:39 am
#198189
Hi
I have a sparkfun esp32 and i am having problems programming when it is connected with a big easy stepper driver when it it powered.
i have switched the pins around now they are connected to
#define DIR 14
#define STEP 32
#define ENABLE 25
#define MS1 13
#define MS2 12
#define MS3 33
so when powered i get the message:
any ideas why i am having these issues?
I have a sparkfun esp32 and i am having problems programming when it is connected with a big easy stepper driver when it it powered.
i have switched the pins around now they are connected to
#define DIR 14
#define STEP 32
#define ENABLE 25
#define MS1 13
#define MS2 12
#define MS3 33
so when powered i get the message:
Code: Select all
and it does not work, when i unplug the power supply of the stepper driver it programs just fine. Uploading 'StepperTest' to 'SparkFun ESP32 Thing' using 'COM13'
Uploader started for board SparkFun ESP32 Thing
Upload method will be: bootloader
Uploading via Bootloader
C:\Users\Danie\Documents\Arduino\hardware\espressif\esp32\tools\esptool.exe --chip esp32 --port "COM13" --baud 921600 --before default_reset --after hard_reset write_flash -z --flash_mode dio --flash_freq 80m --flash_size detect 0xe000 C:\Users\Danie\DOCUME~1\Arduino\hardware\ESPRES~1\esp32/tools/PARTIT~1/BOOT_A~1.BIN 0x1000 C:\Users\Danie\DOCUME~1\Arduino\hardware\ESPRES~1\esp32/tools/sdk/bin/BOOTLO~2.BIN 0x10000 C:\Users\Danie\AppData\Local\Temp\VMBuilds\STEPPE~1\ESPRES~1\Release/STEPPE~2.BIN 0x8000 C:\Users\Danie\AppData\Local\Temp\VMBuilds\STEPPE~1\ESPRES~1\Release/STEPPE~1.BIN
esptool.py v2.1
Connecting.....
Chip is ESP32D0WDQ6 (revision 0)
Uploading stub...
Running stub...
Stub running...
Changing baud rate to 921600
Changed.
Configuring flash size...
Auto-detected Flash size: 4MB
Compressed 8192 bytes to 47...
Writing at 0x0000e000... (100 %)
Wrote 8192 bytes (47 compressed) at 0x0000e000 in 0.0 seconds (effective 4096.0 kbit/s)...
Hash of data verified.
Compressed 12304 bytes to 8126...
Writing at 0x00001000... (100 %)
Wrote 12304 bytes (8126 compressed) at 0x00001000 in 0.1 seconds (effective 1036.1 kbit/s)...
Hash of data verified.
Compressed 143184 bytes to 80559...
Writing at 0x00010000... (20 %)
Writing at 0x00014000... (40 %)
Writing at 0x00018000... (60 %)
Writing at 0x0001c000... (80 %)
Writing at 0x00020000... (100 %)
Wrote 143184 bytes (80559 compressed) at 0x00010000 in 1.5 seconds (effective 762.1 kbit/s)...
A fatal error occurred: Timed out waiting for packet header
esptool.py v2.1
Connecting.....
Chip is ESP32D0WDQ6 (revision 0)
Uploading stub...
Running stub...
Stub running...
Changing baud rate to 921600
Changed.
Configuring flash size...
Auto-detected Flash size: 4MB
Compressed 8192 bytes to 47...
Writing at 0x0000e000... (100 %)
Wrote 8192 bytes (47 compressed) at 0x0000e000 in 0.0 seconds (effective 4096.0 kbit/s)...
Hash of data verified.
Compressed 12304 bytes to 8126...
Writing at 0x00001000... (100 %)
Wrote 12304 bytes (8126 compressed) at 0x00001000 in 0.1 seconds (effective 1036.1 kbit/s)...
Hash of data verified.
Compressed 143184 bytes to 80559...
Writing at 0x00010000... (20 %)
Writing at 0x00014000... (40 %)
Writing at 0x00018000... (60 %)
Writing at 0x0001c000... (80 %)
Writing at 0x00020000... (100 %)
Wrote 143184 bytes (80559 compressed) at 0x00010000 in 1.5 seconds (effective 762.1 kbit/s)...
A fatal error occurred: Timed out waiting for packet header
any ideas why i am having these issues?