Want to switch a set of lights with a servo’s

Have questions about a SparkFun product or board? This is the place to be.

Moderators: phalanx, TS-Tim

Post Reply
NGwpower
Posts: 1
Joined: Tue Dec 26, 2017 2:39 pm

Want to switch a set of lights with a servo’s

Post by NGwpower » Tue Dec 26, 2017 3:14 pm

Have two 110V wall outlets for ceiling lighting, they are blocked by a ho scale train layout. Found a 3D printable wall switch mountable device that uses a servo to throw the switch. Purchased a SparkFun Servo Trigger - Continuous Rotation, let the smoke out of the resistor, wired it to a 12V source! Looking at different offerings from SparkFun:
Goal need the servo to generate at least 180-degree arch.
Will use a momentary switch to operate device.
1. SparkFun Servo Trigger - Continuous Rotation will do 360. Limit is it will only run one servo?
2. SparkFun Servo Trigger – does not go 90 degrees.
3. SparkFun Pi Servo HAT – Prefer not having to use arduino.
Can solder and have multimeter, no good at designing electrical equipment.
Could spend a lot of money on TP-Link or other retailers for smart switches, just cannot justify the expense.
The question is can the #1. “SparkFun Servo Trigger - Continuous Rotation” operate more than one servo, without daisy chaining Triggers?
https://www.thingiverse.com/thing:1156995 is the device
All guidance is appreciated.

Post Reply