ADXL362 giving zeros output

Have questions about a SparkFun product or board? This is the place to be.

Moderators: phalanx, TS-Tim

Post Reply
strom_design
Posts: 1
Joined: Thu Nov 02, 2017 1:14 pm

ADXL362 giving zeros output

Post by strom_design » Thu Nov 02, 2017 1:24 pm

Hi, so I wired up an ADXL362 accelerometer to work with an arduino uno. I have the 3.3V output of the arduino connected to the V+ of the sensor, and SCL, CS, MISO, and MOSI going from the arduino pins 10, 11, 12, 13 through a voltage divider down to 3.3V and then into the sensor. See attached images of the circuit. The issue I am having is that the sensor is outputting only zeros for both acceleration and temperature when running the simpleread sketch. I'm not sure what the cause could be, so any advice is appreciated!

Image links:
https://drive.google.com/open?id=1sjXP2 ... ftycuW99aE
https://drive.google.com/open?id=1ViKVm ... iysv8KnY5M
https://drive.google.com/open?id=1DpMlR ... D_mTQIC8ff

Sensor output:
X=0. Y=0. Z=0. TEMP=0
X=0. Y=0. Z=0. TEMP=0
X=0. Y=0. Z=0. TEMP=0
X=0. Y=0. Z=0. TEMP=0
X=0. Y=0. Z=0. TEMP=0

Post Reply