micro:bit breakout boards

Have questions about a SparkFun product or board? This is the place to be.

Moderators: phalanx, TS-Tim

Post Reply
jadudm
Posts: 6
Joined: Wed Jul 07, 2010 11:32 am

micro:bit breakout boards

Post by jadudm » Wed Sep 27, 2017 11:19 am

Hi team,

My question is about the edge connector for the micro:bit breakout.

https://www.sparkfun.com/products/13988

1. What is that part? Can someone help point me at it in a parts catalogue or similar? (The connector itself.)

2. Is there an Eagle/KiCAD/Upverter/Fritzing part for that connector? Again, if so, could someone point me at it?

I'd really like to design (for example) a sewable carrier for the micro:bit, so that a colleague and I can work on some soft-circuit projects with the micro:bit. This would, essentially, be a Lilypad-like carrier for the micro:bit. Yes, it will be bulky. C'est la vie.

Either way, the electrical design isn't hard, but I don't know what the best way to do the design work on that part would be. Given that Sparkfun has designed a few boards (the breakout, the motor/weather "shields", etc.), I'm wondering if someone here might have some pointers/ideas?

Cheers,
Matt

darrellg
Posts: 324
Joined: Fri Oct 17, 2014 10:02 am
Location: Southern California

Re: micro:bit breakout boards

Post by darrellg » Wed Sep 27, 2017 3:15 pm

It's a 0.05-inch (1.27mm) pitch, 2x40 edge connector. Sparkfun has them on back-order, but Adafruit has them in stock, as well as many other sites. Note that the top and bottom side contacts are are the same, and the wide contacts on the Micro:bit use more than one pin.

Post Reply