- Tue Aug 15, 2017 12:49 pm
#195854
Hello,
My first post here, so please bear with me
I have been struggling with some kind of noise issue with my WAV Trigger board (I have tried two boards to try to rule out hardware faults).
I am not 100% sure where to begin, so I guess from the top:
I have several sound files I wish to play that will be controlled by an arduino micro controller. This bit actually works. However I have a noise issue when playing said files.
I have created an example sound in Soundcloud (https://soundcloud.com/oleshobbyblog/noise-combined). The file first plays the output from the WAV Trigger with the noise just trailing it, it then plays the sound as it should be (i.e. the original). The speaker used is a tiny one so the sound is tinny and awful . The issue is the noise heard after the first time the sound plays, there is a distinctly jittery sound.
I have tried several things to remove this, most did not work:
I am at my wits end, and starting to think I will have to resort to using the on board mono amplifier. I thought however I would give it a shot on here, see if anyone had any clever ideas I could test out before throwing in the towel.
Please let me know if you need more input. I was thinking of adding a drawing, but as I have changed the circuit layout so many times trying different things, I am not sure that would be of any use at this point.
One thing I have not tried is upgrading the firmware.. (I do not have the hardware to do this yet, and I am not sure what I am running atm..cards were purchased a few weeks ago). Could it be that simple?
Another thing, might not be related..but then again, I am no expert.. This happens to both WAV Trigger boards. When I power them using 12V through the barrel connector they get REALLY hot after a while. Like burn your finger hot. This happens on the underside of the barrel connector. It doesn't seem to matter if the on-board amplifier is in use or not. Some heat I would understand, but this feels a bit excessive.
Any input is greatly appreciated!
My first post here, so please bear with me
I have been struggling with some kind of noise issue with my WAV Trigger board (I have tried two boards to try to rule out hardware faults).
I am not 100% sure where to begin, so I guess from the top:
I have several sound files I wish to play that will be controlled by an arduino micro controller. This bit actually works. However I have a noise issue when playing said files.
I have created an example sound in Soundcloud (https://soundcloud.com/oleshobbyblog/noise-combined). The file first plays the output from the WAV Trigger with the noise just trailing it, it then plays the sound as it should be (i.e. the original). The speaker used is a tiny one so the sound is tinny and awful . The issue is the noise heard after the first time the sound plays, there is a distinctly jittery sound.
I have tried several things to remove this, most did not work:
- I have tried different sound files
I have tried two different WAV Trigger boards
I have tried different amplifiers, even used USB speakers with a built in amplifier (powered on the same 5V bus as the rest of the circuit)
I have tried messing with the settings in the initfile editor. Almost nothing works
- Using head phones (not really an option as the project calls for the use of speakers, but I did it just as a test)
Using the on-board mono amplifier (I wish to avoid this to minimize the heat on the WAV Trigger, and I want stereo)
Using two power supplies (5V), one for the WAV Trigger, and one for the amplifiers (with common ground)
I am at my wits end, and starting to think I will have to resort to using the on board mono amplifier. I thought however I would give it a shot on here, see if anyone had any clever ideas I could test out before throwing in the towel.
Please let me know if you need more input. I was thinking of adding a drawing, but as I have changed the circuit layout so many times trying different things, I am not sure that would be of any use at this point.
One thing I have not tried is upgrading the firmware.. (I do not have the hardware to do this yet, and I am not sure what I am running atm..cards were purchased a few weeks ago). Could it be that simple?
Another thing, might not be related..but then again, I am no expert.. This happens to both WAV Trigger boards. When I power them using 12V through the barrel connector they get REALLY hot after a while. Like burn your finger hot. This happens on the underside of the barrel connector. It doesn't seem to matter if the on-board amplifier is in use or not. Some heat I would understand, but this feels a bit excessive.
Any input is greatly appreciated!