- Tue Apr 25, 2017 6:19 pm
#194533
Hi.
I have been unable to use interrupts on the Arduino UNO when the Xbee shield is connected. It's not an issue without the shield. I understand that the Xbee shield has a switch to choose between pins 0 and 1 or pins 2 and 3 for serial transmission, and I have it set up to pins 0 and 1, so that should not be interfering with interrupts on pins 2 and 3 on the UNO. I'm completely stumped as to why I am having this issue...
Any help or suggestion would be greatly appreciated!
I have been unable to use interrupts on the Arduino UNO when the Xbee shield is connected. It's not an issue without the shield. I understand that the Xbee shield has a switch to choose between pins 0 and 1 or pins 2 and 3 for serial transmission, and I have it set up to pins 0 and 1, so that should not be interfering with interrupts on pins 2 and 3 on the UNO. I'm completely stumped as to why I am having this issue...
Any help or suggestion would be greatly appreciated!