- Wed Mar 29, 2017 6:36 pm
#194176
Hi,
I have a sparkfun PRT-13856 Lipo battery pack ( https://www.digikey.com/product-detail/ ... ND/6605200 ) and am attempting to build a charging circuit with the LT3650 charger IC ( https://www.digikey.com/product-detail/ ... ND/2138773 ). My circuit is based on the sample application outlined on page 18 of the IC datasheet, with the exception that I've eliminated the suggested UVLO circuitry (SHDN and CLP are wired to VIN, TIMER is wired to GND and RNG/SS is .1uf to GND). According to the datasheet, this configuration should charge at a max rate of 2A up to C/10.
For prototyping, I have the IC soldered to a SMD breakout board (MSOP-12), and everything wired up on a breadboard with VIN as the 12V out from an old ATX computer power supply (measures ~11.3V). Everything appears to power up properly- the LED which I have connected to the CHG pin lights up, and FAULT does not- and I can measure 4.2V being sent to the BAT pin with the battery disconnected. However, after running the battery down until it shuts off (reads 0V), and then connecting it to the charge circuit in series with an ammeter, I am seeing a current of only ~20-30ma- a far cry from the expected 2A. I had expected to see *some * inefficiencies due to the breadboard wires, less than ideal layout, etc., but not a factor of 100?? The battery does eventually charge up, but being that it is a 6000ma pack, it literally takes SEVERAL DAYS at this 20-30ma rate.
This being my first attempt to build a Lipo charger circuit, I'm sure I'm missing something obvious and/or simple. I double checked the recommended specs. for the SENSE inductor/resistor, and replaced the initial inductor that I was using with another one that better matched the recommended specs.- but still no material difference in the observed charge rate. I also realize that this IC says that it is designed as a "single cell" charger, however, as I understand it, this pack is supposed to be "balanced", and therefore a "single cell" charger should still work, correct? Also, I see from the battery datasheet that it also contains a "protection IC" (DW01+), so perhaps that is somehow limiting the charger current? However, the battery datasheet also recommends a charge rate of 1200ma, so it seems unlikely that it would limit it all the way down to 20ma?
Any ideas would be appreciated- if I can't figure it out, I plan on contacting the IC manufacturer for help next.
Does anyone else have any experience with this particular charging IC and/or chraging circuitry for this battery pack? Any other charger IC/circuits that anyone can recommend that I can use to charge this pack at about a 2A rate with a 12V input?
Thanks in advance!
I have a sparkfun PRT-13856 Lipo battery pack ( https://www.digikey.com/product-detail/ ... ND/6605200 ) and am attempting to build a charging circuit with the LT3650 charger IC ( https://www.digikey.com/product-detail/ ... ND/2138773 ). My circuit is based on the sample application outlined on page 18 of the IC datasheet, with the exception that I've eliminated the suggested UVLO circuitry (SHDN and CLP are wired to VIN, TIMER is wired to GND and RNG/SS is .1uf to GND). According to the datasheet, this configuration should charge at a max rate of 2A up to C/10.
For prototyping, I have the IC soldered to a SMD breakout board (MSOP-12), and everything wired up on a breadboard with VIN as the 12V out from an old ATX computer power supply (measures ~11.3V). Everything appears to power up properly- the LED which I have connected to the CHG pin lights up, and FAULT does not- and I can measure 4.2V being sent to the BAT pin with the battery disconnected. However, after running the battery down until it shuts off (reads 0V), and then connecting it to the charge circuit in series with an ammeter, I am seeing a current of only ~20-30ma- a far cry from the expected 2A. I had expected to see *some * inefficiencies due to the breadboard wires, less than ideal layout, etc., but not a factor of 100?? The battery does eventually charge up, but being that it is a 6000ma pack, it literally takes SEVERAL DAYS at this 20-30ma rate.
This being my first attempt to build a Lipo charger circuit, I'm sure I'm missing something obvious and/or simple. I double checked the recommended specs. for the SENSE inductor/resistor, and replaced the initial inductor that I was using with another one that better matched the recommended specs.- but still no material difference in the observed charge rate. I also realize that this IC says that it is designed as a "single cell" charger, however, as I understand it, this pack is supposed to be "balanced", and therefore a "single cell" charger should still work, correct? Also, I see from the battery datasheet that it also contains a "protection IC" (DW01+), so perhaps that is somehow limiting the charger current? However, the battery datasheet also recommends a charge rate of 1200ma, so it seems unlikely that it would limit it all the way down to 20ma?
Any ideas would be appreciated- if I can't figure it out, I plan on contacting the IC manufacturer for help next.
Does anyone else have any experience with this particular charging IC and/or chraging circuitry for this battery pack? Any other charger IC/circuits that anyone can recommend that I can use to charge this pack at about a 2A rate with a 12V input?
Thanks in advance!