- Wed Mar 08, 2017 2:52 pm
#193792
Hi
I'm building a tracker using a FONA 808 (https://learn.adafruit.com/adafruit-fon ... t/overview) to which I have a LiPO connected. It in turn is connected directly to an arduino pro mini, to the raw pin. I would like to use a Wake on Shake to signal an interrupt using the digital pin #3 on the arduino, rather than having the Wake on Shake power it. Thus I have connected the VIN on the WoS to the VCC of the Arduino, and the VOUT of the WoS to the digital pin #3 of the arduino.
It does not seem to be working though, even after the WoS goes to sleep (I use the serial console issuing the z command to be sure) the voltage on the VOUT pin of the WoS remains at 3.3V. It does eventually go down to 0V but it takes minutes, not the 5 seconds to which it is set by default. Like 1-2 minutes after the unit goes to sleep it will lower the voltage on VOUT. The WAKE pin is connected to digital out #11 of the pro mini, and it is set to LOW.
Is there some strange way in which I could have crossed some wires that could cause this behavior?
Edit: It does appear as though the shake sensor is working, since once it finally lowers the voltage I can turn it back on by moving it around a bit.
I'm building a tracker using a FONA 808 (https://learn.adafruit.com/adafruit-fon ... t/overview) to which I have a LiPO connected. It in turn is connected directly to an arduino pro mini, to the raw pin. I would like to use a Wake on Shake to signal an interrupt using the digital pin #3 on the arduino, rather than having the Wake on Shake power it. Thus I have connected the VIN on the WoS to the VCC of the Arduino, and the VOUT of the WoS to the digital pin #3 of the arduino.
It does not seem to be working though, even after the WoS goes to sleep (I use the serial console issuing the z command to be sure) the voltage on the VOUT pin of the WoS remains at 3.3V. It does eventually go down to 0V but it takes minutes, not the 5 seconds to which it is set by default. Like 1-2 minutes after the unit goes to sleep it will lower the voltage on VOUT. The WAKE pin is connected to digital out #11 of the pro mini, and it is set to LOW.
Is there some strange way in which I could have crossed some wires that could cause this behavior?
Edit: It does appear as though the shake sensor is working, since once it finally lowers the voltage I can turn it back on by moving it around a bit.