SparkFun Forums 

Where electronics enthusiasts find answers.

Have questions about a SparkFun product or board? This is the place to be.
By dorongutman
#192690
Hello,

Either I don't understand how is it supposed to work and how to operate it, or something's not working in my new Sunny Buddy.
I have a 2 watt solar panel (https://www.sparkfun.com/products/13781), the Sunny Buddy v13, and a 3.7v 2000mah LiPo battery (the one that comes with the Particle Electron Asset Tracker (https://store.particle.io/products/asset-tracker), which is labeled PKCELL LR103450).

Before connecting the Lipo battery, I checked its voltage and it was 3.97v.
I connected only the solar panel, checked the SET voltage and changed the potentiometer until it was 3v - just like explained in the hooku guide - https://learn.sparkfun.com/tutorials/su ... king-it-up.

I connected the battery and even after a few hours its voltage hasn't changed from 3.97v.
Later that day, when I didn't have a direct line from the sun, but did have a very good reflection from the buildings around, I checked the SET, CHARGE, FAULT and the cell output itself, and got the following:
Cell - 6.45v
SET - ~2.8v
CHARGE - 3.94v
FAULT - 3.94v

Sometimes, I saw the CHARGE has dropped to 0.03v-0.04v which jumped back to 3.94v when I put my hand over the cell (hiding the light). Sometimes it went back to 0.04v when I removed my hand, sometimes it didn't.
FAULT always stayed at 3.94v.

So... what is going on ?
What am I doing wrong ?
What do I need to tweak ?
Is my Sunny Buddy broken ?

Thanks for the help.
By jremington
#192694
See the LT3652 data sheet for an explanation of the outputs. When /CHARGE and /FAULT are both high, the charger is not charging.

Evidently it thinks the cell is fully charged, which, when the cell has an open circuit voltage of 3.94 volts, is about right. LiPo cells are fully discharged at around 3.2 V and should never be permitted to go much lower than that, or higher than 4.2 V.