SparkFun Forums 

Where electronics enthusiasts find answers.

Have questions about a SparkFun product or board? This is the place to be.
By Mdbirley
#192547
Hi all

The manual for the MG2639 states
The RSSI_LED is driven at high level.
---Power-on status: the LED turns off;
---Network searching status: the LED blinks at 3Hz; ---Idle status: the LED blinks at 1Hz;
---Traffic status (call, data): the LED blinks at 5Hz.

I have installed a talk, text and data AT&T sim in the unit. The LED flashes @ 3 Hz or is off. I does not flash @ 1 Hz or 5 hz ie connected and communicating.

I live in a good signal area and also use another AT&T sim in my conventional phone and this works well.

I took the unit to a AT&T store and we did manage to use the sms auto responder program (so the code is working)
The Getinfo code seems to work fine

When I returned home from the AT&T store No Go the auto responder will not respond

I checked the IMEI number on the unit and with AT&T and they are the same.

The sim has no problems with money as it is on a separate AT&T $45 plan

Any ideas of what to try next

Max