- Sun Jul 10, 2016 8:18 am
#190602
I am wondering how to enable/ disable the Oscillator on the DS3234 RTC breakout. Does the SQW pin need to be grounded?
I would like to be able to use the clock as a second counter for UNIX time or a typical clock giving "human" time.
The example code below is what I am using and it works great, but after a few days the time drifts off. I am not sure if that is due to a communication error over SPI or simply because I don't have the RTC configured correctly.
Any knowledge on this topic would be greatly appreciated!
I would like to be able to use the clock as a second counter for UNIX time or a typical clock giving "human" time.
The example code below is what I am using and it works great, but after a few days the time drifts off. I am not sure if that is due to a communication error over SPI or simply because I don't have the RTC configured correctly.
Code: Select all
Do I simply need to change this line : "SPI.transfer(0x60); //60= disable Osciallator and Battery SQ wave @1hz, temp compensation, Alarms disabled"#include <SPI.h>
const int cs=8; //chip select
void setup() {
Serial.begin(9600);
RTC_init();
//day(1-31), month(1-12), year(0-99), hour(0-23), minute(0-59), second(0-59)
SetTimeDate(11,12,13,14,15,16);
}
void loop() {
Serial.println(ReadTimeDate());
delay(1000);
}
//=====================================
int RTC_init(){
pinMode(cs,OUTPUT); // chip select
// start the SPI library:
SPI.begin();
SPI.setBitOrder(MSBFIRST);
SPI.setDataMode(SPI_MODE1); // both mode 1 & 3 should work
//set control register
digitalWrite(cs, LOW);
SPI.transfer(0x8E);
SPI.transfer(0x60); //60= disable Osciallator and Battery SQ wave @1hz, temp compensation, Alarms disabled
digitalWrite(cs, HIGH);
delay(10);
}
//=====================================
int SetTimeDate(int d, int mo, int y, int h, int mi, int s){
int TimeDate [7]={s,mi,h,0,d,mo,y};
for(int i=0; i<=6;i++){
if(i==3)
i++;
int b= TimeDate[i]/10;
int a= TimeDate[i]-b*10;
if(i==2){
if (b==2)
b=B00000010;
else if (b==1)
b=B00000001;
}
TimeDate[i]= a+(b<<4);
digitalWrite(cs, LOW);
SPI.transfer(i+0x80);
SPI.transfer(TimeDate[i]);
digitalWrite(cs, HIGH);
}
}
//=====================================
String ReadTimeDate(){
String temp;
int TimeDate [7]; //second,minute,hour,null,day,month,year
for(int i=0; i<=6;i++){
if(i==3)
i++;
digitalWrite(cs, LOW);
SPI.transfer(i+0x00);
unsigned int n = SPI.transfer(0x00);
digitalWrite(cs, HIGH);
int a=n & B00001111;
if(i==2){
int b=(n & B00110000)>>4; //24 hour mode
if(b==B00000010)
b=20;
else if(b==B00000001)
b=10;
TimeDate[i]=a+b;
}
else if(i==4){
int b=(n & B00110000)>>4;
TimeDate[i]=a+b*10;
}
else if(i==5){
int b=(n & B00010000)>>4;
TimeDate[i]=a+b*10;
}
else if(i==6){
int b=(n & B11110000)>>4;
TimeDate[i]=a+b*10;
}
else{
int b=(n & B01110000)>>4;
TimeDate[i]=a+b*10;
}
}
temp.concat(TimeDate[4]);
temp.concat("/") ;
temp.concat(TimeDate[5]);
temp.concat("/") ;
temp.concat(TimeDate[6]);
temp.concat(" ") ;
temp.concat(TimeDate[2]);
temp.concat(":") ;
temp.concat(TimeDate[1]);
temp.concat(":") ;
temp.concat(TimeDate[0]);
return(temp);
}
Any knowledge on this topic would be greatly appreciated!