- Fri Mar 11, 2016 5:09 pm
#188632
I received two of these boards today and neither one will upload blink or any other example sketch. The boards show up as com41 or com42 depending on which one is plugged in. The baud value is set to 115200 on the comport and matches the value the uploader wants to use. Nothing else is using the port but the upload makes nine attempts and blinks the light then fails with the following message. I tried to update the driver but W7-64 shows a window that says it's downloading the driver file but never completes. At this point, I would prefer to return the boards as opposed to cutting traces and installing jumpers. If this is what you have to do to get it working then the product is not really reading for sale.
Code: Select all
Sketch uses 219,267 bytes (50%) of program storage space. Maximum is 434,160 bytes.
Global variables use 31,464 bytes (38%) of dynamic memory, leaving 50,456 bytes for local variables. Maximum is 81,920 bytes.
C:\Users\xxxx\AppData\Roaming\Arduino15\packages\esp8266\tools\esptool\0.4.8/esptool.exe -vv -cd nodemcu -cb 115200 -cp COM42 -ca 0x00000 -cf C:\Users\xxxx\AppData\Local\Temp\build507896959865733368.tmp/Blink.cpp.bin
esptool v0.4.8 - (c) 2014 Ch. Klippel <ck@atelier-klippel.de>
setting board to nodemcu
setting baudrate from 115200 to 115200
setting port from COM1 to COM42
setting address from 0x00000000 to 0x00000000
espcomm_upload_file
espcomm_upload_mem
setting serial port timeouts to 1000 ms
opening bootloader
resetting board
trying to connect
flush start
setting serial port timeouts to 1 ms
setting serial port timeouts to 1000 ms
flush complete
espcomm_send_command: sending command header
espcomm_send_command: sending command payload
read 0, requested 1
trying to connect
flush start
setting serial port timeouts to 1 ms
setting serial port timeouts to 1000 ms
flush complete
espcomm_send_command: sending command header
espcomm_send_command: sending command payload
read 0, requested 1
trying to connect
flush start
setting serial port timeouts to 1 ms
setting serial port timeouts to 1000 ms
flush complete
espcomm_send_command: sending command header
espcomm_send_command: sending command payload
read 0, requested 1
resetting board
trying to connect
flush start
setting serial port timeouts to 1 ms
setting serial port timeouts to 1000 ms
flush complete
espcomm_send_command: sending command header
espcomm_send_command: sending command payload
read 0, requested 1
trying to connect
flush start
setting serial port timeouts to 1 ms
setting serial port timeouts to 1000 ms
flush complete
espcomm_send_command: sending command header
espcomm_send_command: sending command payload
read 0, requested 1
trying to connect
flush start
setting serial port timeouts to 1 ms
setting serial port timeouts to 1000 ms
flush complete
espcomm_send_command: sending command header
espcomm_send_command: sending command payload
read 0, requested 1
resetting board
trying to connect
flush start
setting serial port timeouts to 1 ms
setting serial port timeouts to 1000 ms
flush complete
espcomm_send_command: sending command header
espcomm_send_command: sending command payload
read 0, requested 1
trying to connect
flush start
setting serial port timeouts to 1 ms
setting serial port timeouts to 1000 ms
flush complete
espcomm_send_command: sending command header
espcomm_send_command: sending command payload
read 0, requested 1
trying to connect
flush start
setting serial port timeouts to 1 ms
setting serial port timeouts to 1000 ms
flush complete
espcomm_send_command: sending command header
espcomm_send_command: sending command payload
read 0, requested 1
warning: espcomm_sync failed
error: espcomm_open failed
error: espcomm_upload_mem failed