- Wed Apr 01, 2015 1:31 pm
#180882
Hi,
I'm playing with a brand new Fio v3 and I can't seem to get any code to upload. I've been doing the proper double-tap reset, but I keep getting a jssc.SerialPortException saying "Port Busy". The port (/dev/ttyACM0) is the correct one and I have installed all of the proper board definitions.
Setup:
Any ideas?
I'm playing with a brand new Fio v3 and I can't seem to get any code to upload. I've been doing the proper double-tap reset, but I keep getting a jssc.SerialPortException saying "Port Busy". The port (/dev/ttyACM0) is the correct one and I have installed all of the proper board definitions.
Setup:
- Arduino 1.6.2
- Fedora 21
- Fio v3
- USB (i.e. not XBee)
processing.app.debug.RunnerExceptionThe port (/dev/ttyACM0) shows up in the /dev directory when the Fio is connected (it is the port I typically see for ATMega32U4-based boards), but it does not show up in the Arduino IDE.
at cc.arduino.packages.uploaders.SerialUploader.uploadUsingPreferences(SerialUploader.java:133)
at processing.app.debug.Compiler.upload(Compiler.java:158)
at processing.app.Sketch.upload(Sketch.java:1260)
at processing.app.Sketch.exportApplet(Sketch.java:1202)
at processing.app.Sketch.exportApplet(Sketch.java:1174)
at processing.app.Editor$DefaultExportHandler.run(Editor.java:2471)
at java.lang.Thread.run(Thread.java:745)
Caused by: processing.app.SerialException: Error touching serial port '/dev/ttyACM0'.
at processing.app.Serial.touchForCDCReset(Serial.java:92)
at cc.arduino.packages.uploaders.SerialUploader.uploadUsingPreferences(SerialUploader.java:122)
... 6 more
Caused by: jssc.SerialPortException: Port name - /dev/ttyACM0; Method name - openPort(); Exception type - Port busy.
at jssc.SerialPort.openPort(SerialPort.java:164)
at processing.app.Serial.touchForCDCReset(Serial.java:86)
... 7 more
Any ideas?