- Tue Feb 17, 2015 7:43 pm
#179838
I also am having trouble getting the motor to run as fast as I want . I’m using the sparkfun NEMA17 motors but have tried others too. My motors are rotating about 1-2 rev / sec. I’m using the accelstepper library (see below) code but have also used other code (stepper library).
I’m following the diagram for jumping the microstep pins to ground to set the resolution to FULL STEP (MS1, MS2, and MS3 jumped to Ground) assuming FULL STEP means quickest speed (right?)
However the motors run really slow (like 10 RPM) , but when MS1 is jumped to ground and MS3 and MS2 are floating it seems to run about 1-2 rev/sec but that’s still too slow. I assume I can run these motors much faster and I’m not understanding something about the motor driver.
FYI using arduino w/ library accelstepper : this is what I have in the loop stepper.setMaxSpeed(20000); stepper.setSpeed(20000); stepper.runSpeed();
I’m following the diagram for jumping the microstep pins to ground to set the resolution to FULL STEP (MS1, MS2, and MS3 jumped to Ground) assuming FULL STEP means quickest speed (right?)
However the motors run really slow (like 10 RPM) , but when MS1 is jumped to ground and MS3 and MS2 are floating it seems to run about 1-2 rev/sec but that’s still too slow. I assume I can run these motors much faster and I’m not understanding something about the motor driver.
FYI using arduino w/ library accelstepper : this is what I have in the loop stepper.setMaxSpeed(20000); stepper.setSpeed(20000); stepper.runSpeed();