- Sat Jan 31, 2015 2:29 pm
#179326
I'm trying to use the VCC output of a Sparkfun PowerCell to drive the 5V DC (168 ohm) coil of a DPDT relay. The relay is supposed to be energized whenever the PowerCell has 5V applied, either via the USB connector or via the 5V input. However, at least with the unit I have here, it doesn't work.
If I drive the relay with a 5V lab power supply, it works fine and exhibit the appropriate current flow for a 168-ohm coil resistance (approx 30mA).
If I leave one wire to the relay coil disconnected so I can first make the USB connection and then apply VCC to the relay, it works fine (I can hear the relay click and measure the change in contact connections).
if I connect both wires (VCC and GND) to the relay coil, and then plug in the USB connector, the relay does not engage (no sound, no change in contact connections)
What gives here - is there some startup problem with the PowerCell with inductive loads? Is there any workaround to this issue?
TIA,
Frank
If I drive the relay with a 5V lab power supply, it works fine and exhibit the appropriate current flow for a 168-ohm coil resistance (approx 30mA).
If I leave one wire to the relay coil disconnected so I can first make the USB connection and then apply VCC to the relay, it works fine (I can hear the relay click and measure the change in contact connections).
if I connect both wires (VCC and GND) to the relay coil, and then plug in the USB connector, the relay does not engage (no sound, no change in contact connections)
What gives here - is there some startup problem with the PowerCell with inductive loads? Is there any workaround to this issue?
TIA,
Frank