- Fri Nov 14, 2014 4:37 pm
#176895
Yeah yeah yeah, I know, no support for parts obtained in the dumpster dive, blah blah blah.
I received this in the last dumpster dive. I can't find anything wrong with it visually (it came in an already-opened package with headers soldered on), so I tried powering it up. Nothing showed on the display. I tested one segment and it lit up. It looks just like the one in the product picture, 'cept for the numbers on the bottom of the ATMega saying "1223".
There are a few things I can think of that could be wrong with it: broken traces hidden under the display, the ATMega not being programmed (or not having a boot loader, even), or just a dead ATMega. I actually want to salvage the thing if I can. So the question comes down to this. Where what and how should I test the board to see where the problem lies? I have a DMM, a pocket o-scope, and two Arduino UNOs.
*EDIT*
The resistors are showing about 1K of resistance. I know the Mega is getting power (I got the Eagle files). I have not tested all of the traces yet, though.
I received this in the last dumpster dive. I can't find anything wrong with it visually (it came in an already-opened package with headers soldered on), so I tried powering it up. Nothing showed on the display. I tested one segment and it lit up. It looks just like the one in the product picture, 'cept for the numbers on the bottom of the ATMega saying "1223".
There are a few things I can think of that could be wrong with it: broken traces hidden under the display, the ATMega not being programmed (or not having a boot loader, even), or just a dead ATMega. I actually want to salvage the thing if I can. So the question comes down to this. Where what and how should I test the board to see where the problem lies? I have a DMM, a pocket o-scope, and two Arduino UNOs.
*EDIT*
The resistors are showing about 1K of resistance. I know the Mega is getting power (I got the Eagle files). I have not tested all of the traces yet, though.
Code: Select all
<?php
while(1){
echo "Hey, wait! This is a trap!";
}
?>