- Tue Aug 08, 2006 4:48 pm
#16919
hi
well i have an application where a very tiny pic based circuit is being used.
it is in sleep mode all day using less than 10uA. but once in a day it wakes up for a minute, uses 20mA(max) for the whole minute and then goes to sleep for another 24 hours.
as these are disposible, i am thinking of using a small solar cell and charging a capacitor. within the 24 hours. then using the capacitors charge to run the circuit for that minute. thus using no battery at all and getting much longer life than i would get from a button cell. overall size is very restricted. is that possible. can i have a circuit example for the power side of it. and also, how can i calculate the charge capacity for the capacitor for this applicaiton.
thanks
well i have an application where a very tiny pic based circuit is being used.
it is in sleep mode all day using less than 10uA. but once in a day it wakes up for a minute, uses 20mA(max) for the whole minute and then goes to sleep for another 24 hours.
as these are disposible, i am thinking of using a small solar cell and charging a capacitor. within the 24 hours. then using the capacitors charge to run the circuit for that minute. thus using no battery at all and getting much longer life than i would get from a button cell. overall size is very restricted. is that possible. can i have a circuit example for the power side of it. and also, how can i calculate the charge capacity for the capacitor for this applicaiton.
thanks