- Tue Jun 24, 2014 11:06 pm
#172206
Did the recording tonight and I learned several things:
-The 4th position on the 4: line is the oil temp
-There are timing issues/parsing issues with repeatedly resetting the header to default and back to 7E0. An OK gets returned from the chip which includes an \0 or \n character which causes the "dumb" parsing of the return to end reading the buffer. I'll have to make the parsing more intelligent. Skip any OK's and look specifically at the 4: line and not at a specific spacing in the return.
-The 4th position on the 4: line is the oil temp
-There are timing issues/parsing issues with repeatedly resetting the header to default and back to 7E0. An OK gets returned from the chip which includes an \0 or \n character which causes the "dumb" parsing of the return to end reading the buffer. I'll have to make the parsing more intelligent. Skip any OK's and look specifically at the 4: line and not at a specific spacing in the return.