- Thu Apr 17, 2014 7:23 pm
#170356
I'm having trouble programming my new RedBot mainboard. I'm on OS X using the Arduino IDE 1.0.5. When I hook it up to the USB cable, the power light comes on as expected. I select the /dev/tty.usbserial-XXXXXXXX port and set the board to be an Arduino Uno. When I try to program the board, it hangs. The RX light on the board is continually flashing, but nothing seems to happen.
I get the same behavior when trying to upload just the blink sketch. I bought several boards and have gotten the same behavior from the two I've tried.
I've also got a Duemilanove that I can program on the same Mac without a problem.
Any pointers?
Thanks!
I get the following verbose output from the IDE:
I get the same behavior when trying to upload just the blink sketch. I bought several boards and have gotten the same behavior from the two I've tried.
I've also got a Duemilanove that I can program on the same Mac without a problem.
Any pointers?
Thanks!
I get the following verbose output from the IDE:
Code: Select all
Binary sketch size: 1,084 bytes (of a 32,256 byte maximum)
/Users/awillis/Applications/Arduino.app/Contents/Resources/Java/hardware/tools/avr/bin/avrdude -C/Users/awillis/Applications/Arduino.app/Contents/Resources/Java/hardware/tools/avr/etc/avrdude.conf -v -v -v -v -patmega328p -carduino -P/dev/tty.usbserial-A603G8J2 -b115200 -D -Uflash:w:/var/folders/7c/gz4cjjxn7pj9pg_8grtwq9mrxjzwjk/T/build9154817360580079835.tmp/Blink.cpp.hex:i
avrdude: Version 5.11, compiled on Sep 2 2011 at 18:52:52
Copyright (c) 2000-2005 Brian Dean, http://www.bdmicro.com/
Copyright (c) 2007-2009 Joerg Wunsch
System wide configuration file is "/Users/awillis/Applications/Arduino.app/Contents/Resources/Java/hardware/tools/avr/etc/avrdude.conf"
User configuration file is "/Users/awillis/.avrduderc"
User configuration file does not exist or is not a regular file, skipping
Using Port : /dev/tty.usbserial-A603G8J2
Using Programmer : arduino
Overriding Baud Rate : 115200