- Wed Jul 26, 2006 9:40 am
#16266
I have a small battery (3.3V) operated circuit that I want to add a voltage level feature to.
I want to occasionally measure the battery voltage level using the MCU's ADC. The adc input pin is high impedance however I don't want to directly provide a 3.3V connection to it all the time as it will drain the battery fairly quickly. I was wondering if there are any small switches out there which I could control through another IO line which can be kept open for the most part but can be switched on for a short time when trying to calculate the voltage level.
Important factors for this part will be size and cost, cheap as heck and 'VERY' tiny as I'm severely restricted by board space.
Any ideas?
I want to occasionally measure the battery voltage level using the MCU's ADC. The adc input pin is high impedance however I don't want to directly provide a 3.3V connection to it all the time as it will drain the battery fairly quickly. I was wondering if there are any small switches out there which I could control through another IO line which can be kept open for the most part but can be switched on for a short time when trying to calculate the voltage level.
Important factors for this part will be size and cost, cheap as heck and 'VERY' tiny as I'm severely restricted by board space.
Any ideas?