- Wed Jan 22, 2014 10:56 pm
#167549
I recently purchased the RS232 Shifter SMD No DB9,PRT-08780.
I am wanting to use it to add Bluetooth connectivity to a microcontroller based box I'm using. Can someone verify that this is an intended use for this product?
Here is how it is connected:
The microcontroller has its com lines running through a MAX232 chip and out to a DB9 connector. It is intended to be connected to a PC serial port. I wanted to use one of those cheap eBay Bluetooth modules(5v supply, 3.3v level TX/RX) to connect wirelessly. I connected the shifter board to the db9 on the box via a gender changer since they both have female connectors. I connected 5v to the Bluetooth module via pin 1 on the db9(supplied by the box) then added a voltage divider to get 3.3v on the VCC pin on the shifter board (3.26v confirmed with DMM). I connected TX on the shifter to RX on the BT module and vice versa. Every thing would power up and I could pair to the BT but it seemed like I couldn't get any serial comms though to the micro box at all. I even tried reversing the TX/RX connections with no change.
Am I missing something or is this shifter board not meant to be used like this?
I am wanting to use it to add Bluetooth connectivity to a microcontroller based box I'm using. Can someone verify that this is an intended use for this product?
Here is how it is connected:
The microcontroller has its com lines running through a MAX232 chip and out to a DB9 connector. It is intended to be connected to a PC serial port. I wanted to use one of those cheap eBay Bluetooth modules(5v supply, 3.3v level TX/RX) to connect wirelessly. I connected the shifter board to the db9 on the box via a gender changer since they both have female connectors. I connected 5v to the Bluetooth module via pin 1 on the db9(supplied by the box) then added a voltage divider to get 3.3v on the VCC pin on the shifter board (3.26v confirmed with DMM). I connected TX on the shifter to RX on the BT module and vice versa. Every thing would power up and I could pair to the BT but it seemed like I couldn't get any serial comms though to the micro box at all. I even tried reversing the TX/RX connections with no change.
Am I missing something or is this shifter board not meant to be used like this?