- Mon Jan 27, 2014 11:35 pm
#167788
DCward wrote:Just reconnect the unity gain buffer circuit, the value of the resistor, capacitor is the same as the what Mee_n_Mac drew.So within 0.1v of what it should. Given the tolerances involved, I'd say it's working.
...
when the supply is around 9.2v to the circuit, using the 100 ohms burden, the circuit output is 4.90vdc
DCward wrote:For the circuit output current, with 250ohms resistor connecting the output, both 100ohms and 4.5kohms burden give around 10mAThat's odd as the min current spec for your LM324 is 20 mA. How sure are you about that 10mA and/or that the total load was 250 ohms ? That the output was still 5v with the 250 ohm resistor load ?