- Sat Apr 20, 2013 2:58 pm
#158631
I'm designing an Arduino board that is almost completely digital. The analog paths to the analog pins and the atmega324 are the only analog components. It uses 3 voltage levels, 2.5V, 3.3V and 5V. It's a 4 layer board, and I'm wondering what's the best method for providing power and ground. 2.5V is used by one clock and possibly the atmega. 3.3V powers the digital peripherals and possibly the atmega. 5V powers the 5V pin and possibly the atmega. The atmega uses jumpers to select its operating voltage.
I'm thinking about a 4 layer board with top and bottom being signal layers, and the two internal layers being Vcc and GND. I read in a TI app note on analog digital that it's best to have a continuous ground plane split in to analog zones. I'm not sure I need that for the atmega chip, it's the only analog thing on the board. I'm also thinking of using the Vcc plane to route power on a trace by trace basis(maybe with fills), Is this reasonable? Do I need to worry about signal path like I do for the ground plane? I can use the same ground for multiple voltage levels, right?
Finally, I know vias can run from the top layer through all the layers, blind vias connect two internal layers, and buried vias connect one external layer to a number of internal layers. Is this correct?
I'm thinking about a 4 layer board with top and bottom being signal layers, and the two internal layers being Vcc and GND. I read in a TI app note on analog digital that it's best to have a continuous ground plane split in to analog zones. I'm not sure I need that for the atmega chip, it's the only analog thing on the board. I'm also thinking of using the Vcc plane to route power on a trace by trace basis(maybe with fills), Is this reasonable? Do I need to worry about signal path like I do for the ground plane? I can use the same ground for multiple voltage levels, right?
Finally, I know vias can run from the top layer through all the layers, blind vias connect two internal layers, and buried vias connect one external layer to a number of internal layers. Is this correct?