- Sun Jan 13, 2013 10:24 pm
#154194
Well, I'm at a loss.... I'm trying to re-purpose an automobile power window motor into a new project. I pulled the switch and motor out of a junked car, but I'm not quite sure what's going on. I tested the switch unit in the vehicle before removing it (stuck a 12 v car battery in, and measured the voltage at the 2 wires coming out of the switch) When the switch was pressed in the "down" position, the multimeter showed 11 to 12 volts. When the switch was pressed in the "up" position it put out -11 to -12 volts, just as you'd expect. Then I tested the motor itself... I pulled it out of the car, and with no load on it, I put 9 volts on the wires leading in and the motor turned clockwise; then I reversed the pos/grnd leads, and the clock turned counter-clockwise... just as it should. The problem comes when I connect the two -- with the switch still connected in the car, I connected the motor to the switch, and the motor turns clockwise when the switch is pressed in the "down" position, but does nothing when the switch is pressed in the "up" position. If I reverse the wire connections, the motor will turn in the opposite direction when the switch is in the "down" position, but still does nothing when the switch is in the "up" position. Now, I know that since the multimeter showed positive and negative voltage coming from the switch, the motor SHOULD be working in both directions, but it refuses to operate when the switch is in the "up" position.... so basically, the switch works as expected in isolation, the motor works as expected in isolation, but once connected, it ain't working... anyone have any idea what I should be looking for --- how do I even decided if the problem is the switch or the motor???????