- Sat Dec 08, 2012 12:28 pm
#152961
Something else I'm not entirely understanding. I learned a long time ago that as voltage goes up, Amps goes down. So, if I'm using two single cell LiPos, 6,600mA each, in parallel, at the point where they are tied together (with diodes), technically I should have 3.7V @ 13,200mA. Yes?
And if I buck/boost that to 5V, is the amount of Amps equally affected, bringing it down to ... uh, I think about 8,712ma?
And if I buck/boost that to 5V, is the amount of Amps equally affected, bringing it down to ... uh, I think about 8,712ma?