- Wed Jul 18, 2012 8:57 am
#147547
First, i'm going to appologize for putting this in this forum, since it is not a sparkfun product, but I don't know where else to ask it.
I just bought the 10dof board from http://www.goodluckbuy.com/10dof-nine-a ... ensor.html. This breakout board appears to have pins that are not described in the datasheet, and not have ones that are described in the datasheet. The pins i'm unsure about are, CLO, CLI, DRY, FYN, ADO, and VLG. I think i can safely assume DRY is the same as DRDY on the datasheet. FYN might be the same as FSYNC, and VLG might be the same as VLOGIC. That still leaves CLO, CLI, and ADO. For my project, i need to be able to tell when each of the sensors has new data. The HMC5883L has the DRDY pin. The MPU6050 has the INT pin (I think. Correct me if i'm wrong). The BMP086 has the EOC pin. Unfortunatedly, i don't know if EOC is broken out. Another problem is with the ASDA and ASCL pins. These pins enable the user to get 9-axis MotionFusion data from the MPU6050 if they are conected to a 3-axis magnetometer. Part of the reason I bought the board is that it has the 3-axis magnetometer on it. Unfortunatly i don't think the SDA and SCL pins on the magnetometer are connected to ASCL and ASDA. Instead, I think they are just connected to the SCL and SDA on the breakout. To make matters worse, when I contacted the company asking for a schematic of the breakout board, they never replied. Could somebody please advise me on what to do.
I just bought the 10dof board from http://www.goodluckbuy.com/10dof-nine-a ... ensor.html. This breakout board appears to have pins that are not described in the datasheet, and not have ones that are described in the datasheet. The pins i'm unsure about are, CLO, CLI, DRY, FYN, ADO, and VLG. I think i can safely assume DRY is the same as DRDY on the datasheet. FYN might be the same as FSYNC, and VLG might be the same as VLOGIC. That still leaves CLO, CLI, and ADO. For my project, i need to be able to tell when each of the sensors has new data. The HMC5883L has the DRDY pin. The MPU6050 has the INT pin (I think. Correct me if i'm wrong). The BMP086 has the EOC pin. Unfortunatedly, i don't know if EOC is broken out. Another problem is with the ASDA and ASCL pins. These pins enable the user to get 9-axis MotionFusion data from the MPU6050 if they are conected to a 3-axis magnetometer. Part of the reason I bought the board is that it has the 3-axis magnetometer on it. Unfortunatly i don't think the SDA and SCL pins on the magnetometer are connected to ASCL and ASDA. Instead, I think they are just connected to the SCL and SDA on the breakout. To make matters worse, when I contacted the company asking for a schematic of the breakout board, they never replied. Could somebody please advise me on what to do.