- Thu Aug 01, 2013 2:55 pm
#162198
I have been able to modulate very cheap laser diodes at 500 MHz on my workbench with an RF signal generator and receive the signal with an OE converter. The next step is to receive the reflected signal with a photodiode detector and low noise amplifier chain. However, isolation and filtering are a big problem and the filter I built did not work (very high loss) because the component values in my assortment were not correctly marked. I got sidetracked trying to come up with a way to accurately measure caps on the order of 1 pF so I could build another filter with the correct component values.
UNTEngineer wrote:I saw that particular product already. I think the links were posted earlier in this same post. It does look like a pretty nice product, but I'm thinking about trying something rather different; using a phase measurement instead of a direct time of flight measurement. I am primarily targeting high precision, short-range measurements so the design space is a little different. For one, I want to use a very basic laser diode. If I can get it to work with a $1 made in china laser diode, then that would simplify construction and part sourcing as well as reduce the price.alex.forencich wrote:I have been mulling this over for a while and I think it may be possible to build a high resolution, high accuracy distance sensor (better than 5mm) with a high update rate (more than 1,000 samples/sec) at a relatively low cost (possibly $200-300) in the form of a laser rangefinder. Operation would be based on transmitting a high frequency modulated laser beam and then measuring the phase shift of the returned light. I will have to work through the design to be sure, but it could well be doable on a single board of about 3x5 in.By the way, you're not the first person to think of this (I myself followed this research some months ago):
http://forums.parallax.com/showthread.p ... nge+finder
And:
http://forums.parallax.com/showthread.p ... evaluation
Its good to note, this project is underway in South Africa. So the founder is having a bunch of problems with US import laws regarding his system. Hes using a high power laser thats not easily available here, so this may be an issue in your project. Im excited to see progress on your project; maybe we can bring the price tag down AND make it available to folks here in the US.
I have been able to modulate very cheap laser diodes at 500 MHz on my workbench with an RF signal generator and receive the signal with an OE converter. The next step is to receive the reflected signal with a photodiode detector and low noise amplifier chain. However, isolation and filtering are a big problem and the filter I built did not work (very high loss) because the component values in my assortment were not correctly marked. I got sidetracked trying to come up with a way to accurately measure caps on the order of 1 pF so I could build another filter with the correct component values.
Alex Forencich