- Thu Nov 17, 2011 5:27 pm
#135879
Hi,
I'm trying to hand assemble a prototype with a few SMDs. They are quite small devices, with up to 8 leads. The method I'm trying to use is to solder a thin tinned copper wire onto each used lead or pad of the SMD, and then use these wires to connect the chip to my prototype board. So far this has been unsuccessful, and has fatally damaged a fairly expensive chip that I've only got one of. This was an LCC8 pack, i.e. a ceramic device that just has 8 plated pads on the bottom of it. It has no physical metal leads - just these plated pads. They are gold, or gold plated. I seemed to solder the wires on successfully, but they pinged off very easily, and in one case they seem to have pulled off or damaged the plated pad. I wonder whether I used too thick a wire, leaving nothing to provide strain relief.
Before I buy another chip and have another go, I need to understand how to do this successfully:
Thanks for your help and advice - Rowan
I'm trying to hand assemble a prototype with a few SMDs. They are quite small devices, with up to 8 leads. The method I'm trying to use is to solder a thin tinned copper wire onto each used lead or pad of the SMD, and then use these wires to connect the chip to my prototype board. So far this has been unsuccessful, and has fatally damaged a fairly expensive chip that I've only got one of. This was an LCC8 pack, i.e. a ceramic device that just has 8 plated pads on the bottom of it. It has no physical metal leads - just these plated pads. They are gold, or gold plated. I seemed to solder the wires on successfully, but they pinged off very easily, and in one case they seem to have pulled off or damaged the plated pad. I wonder whether I used too thick a wire, leaving nothing to provide strain relief.
Before I buy another chip and have another go, I need to understand how to do this successfully:
- What type of solder should I be using? Should it be leaded, or lead free? What should its melting point be? What gauge of solder works best?
- Do I need a separate flux? If so, what sort?
- What temperature should my soldering iron be set to?
- What gauge of wire works best?
- Any other suggestions to make a success of this?
Thanks for your help and advice - Rowan