SparkFun Forums 

Where electronics enthusiasts find answers.

Have questions about a SparkFun product or board? This is the place to be.
#132920
I've recently purchased a Bourns EM14 rotary encoder to play with: http://goo.gl/1PpR5

The 6 pins are spaced at .05", instead of the .1" that I'm used to. Consequently, the component won't fit into any of my breadboards or interconnects.

I'm trying to figure out the best way to jack this component into a prototyping system so I can begin to experiment with it. Any suggestions?

Bourns makes an inexpensive cable that would be perfect (http://goo.gl/y7S0K ) but I can't find anywhere that currently stocks it.

One option would be to just buy a cable connector with the correct pitch and enough channels to accomodate the EM14 (for instance http://goo.gl/odtrd ) but I'm wondering if there's a simpler method that I haven't considered.

Any thoughts would be appreciated, thanks!
#132921
tones,

I don't seem to be able to pull up the datasheets ATM, so I can't see how long the leads are.

If they're long enough, you can bend them to form a 2 X 3 matrix on 0.1 spacing. That doesn't solve your breadboard problem directly, but you could then fit a 2 X 2, 0.1-spaced female connector.

Alternatively, you could bend the pins in alternating directions from the line that passes through them, then attach either individual leads (either leads with female connectors, or by wire wrapping) or 2, 1 X 3, 0.1-spaced connectors.

Eric
#132940
@langwadt:
That's a good point about ribbon cable. Unfortunately, a 2 X 3 connector isn't a convenient thing when working on a breadboard; a 1 X 6 is. One could, however, fan out the ribbon cable to get 0.1 spacing. If the fanned-out leads are tinned heavily enough, they should work in a breadboard.

I was trying to provide a method that doesn't require soldering to the component. Do you think the component's leads could be persuaded to fit into the cable side of a ribbon connector?

Eric
#132971
Instead of using a 2x3 connector, I was thinking I'd just strip the ribbon cables and insert them into the breadboard individually.

Good news though -- I contacted Bourns and they offered to send me a few free samples of their prototyping connector cables. So, problem solved.