- Wed Apr 05, 2006 2:49 pm
#11911
No, modern electrolytics don't dry out. They form an oxide layer inside ove r the course of a year or two in storage, possibly shorter. Especially in higher voltage applications (220V, 480V, etc) this can cause the cap to rupture catastrophically if full voltage and load are applied suddenly. This is also why sometimes if you plug in a piece of equipment that hasn't been run in a few years it'll die suddenly.
They can be reformed, however, back to operation.
FYI: The capacitors I deal with are behind a bridge rectifier (AC variable frequency drives), so we start with a low voltage (40V) from our 3 phase variac and slowly raise the voltage by 20-40V every 10 minutes, usually up to the overvoltage trip point of the drive (close to the max voltage rating of the caps). There's no load and the drive is just idle during this time. The home equivalent would be using a variac or a light dimmer, through a bridge rectifier, into your capacitors (with load resistor so you have an RC circuit going). Start low and raise it slowly to max over the course of an hour (step every 10 minutes). Do NOT do this with your house electronics, though, good chance you might fry something else that doesn't like brownout conditions.
Technical Alchemy
Strange ideas, rambling technical thoughts
http://technicalchemy.blogspot.com/
(yes, I'm working on a real website eventually)