- Sun Feb 20, 2011 2:53 pm
#120768
I thought you guys might be interested in seeing the project we just finished -- a backyard rocketship treehouse.
Rarely does building a treehouse require welding, grinding, painting, riveting, bending, crimping, plumbing, brazing, laser cutting, sound design, printed circuit board fabrication, thousands of lines of C code, distributed network protocols, sewing and embroidery. Ours did.
Here's a video showing it "take off": http://www.youtube.com/watch?v=8izMrzulMHI
Our project web site (http://rocket.jonh.net) has all our schematics and source code, as well.
The rocket is a hexagonal capsule, 7.5 feet (2.3 meters) high, atop a tripod 7.5 feet (2.3 meters) high, for an overall height of about 15 feet (4.6 meters). It is about 6.5 feet (2 meters) across at its widest point. The frame is welded mild steel with riveted aluminum siding. It contains nearly 800 LEDs forming dozens of numeric displays spread across 14 control panels, each with an acrylic face laser-cut and etched with labels such as "Lunar Distance" and "Hydraulic Pressure". The pilot controls the rocket using a joystick and panels full of working switches, knobs and buttons. Underneath the capsule are three "thrusters" that shoot plumes of water and compressed air under the control of the pilot's joystick, simulating real positioning thrusters. Takeoff and docking sequences are augmented by a paint-shaker that simulates the vibration of a rocket engine. Sound effects complete the illusion, with a powered subwoofer that gives the rocket a satisfying rumble.
Behind the scenes, rocket operations are controlled by three Atmega328 microprocessors on custom-fabricated printed circuit boards, running a small operating system, RULOS, that we built just for this project. The processors communicate using an in-rocket TWI network and will eventually talk back to the house over a serial port. A trench running from the house to the rocket carries 12VDC power for the lighting and electronics, water for the thrusters, compressed air, and several data signals.
Cheers,
Jeremy
Rarely does building a treehouse require welding, grinding, painting, riveting, bending, crimping, plumbing, brazing, laser cutting, sound design, printed circuit board fabrication, thousands of lines of C code, distributed network protocols, sewing and embroidery. Ours did.
Here's a video showing it "take off": http://www.youtube.com/watch?v=8izMrzulMHI
Our project web site (http://rocket.jonh.net) has all our schematics and source code, as well.
The rocket is a hexagonal capsule, 7.5 feet (2.3 meters) high, atop a tripod 7.5 feet (2.3 meters) high, for an overall height of about 15 feet (4.6 meters). It is about 6.5 feet (2 meters) across at its widest point. The frame is welded mild steel with riveted aluminum siding. It contains nearly 800 LEDs forming dozens of numeric displays spread across 14 control panels, each with an acrylic face laser-cut and etched with labels such as "Lunar Distance" and "Hydraulic Pressure". The pilot controls the rocket using a joystick and panels full of working switches, knobs and buttons. Underneath the capsule are three "thrusters" that shoot plumes of water and compressed air under the control of the pilot's joystick, simulating real positioning thrusters. Takeoff and docking sequences are augmented by a paint-shaker that simulates the vibration of a rocket engine. Sound effects complete the illusion, with a powered subwoofer that gives the rocket a satisfying rumble.
Behind the scenes, rocket operations are controlled by three Atmega328 microprocessors on custom-fabricated printed circuit boards, running a small operating system, RULOS, that we built just for this project. The processors communicate using an in-rocket TWI network and will eventually talk back to the house over a serial port. A trench running from the house to the rocket carries 12VDC power for the lighting and electronics, water for the thrusters, compressed air, and several data signals.
Cheers,
Jeremy