- Sun Feb 13, 2011 11:39 am
#120171
A highly conductive surface like aluminium isn't static safe; in fact, by providing a low resistance to earth it actually increases the chances of a destructive discharge through the device.
ESD damage occurs when a large current flows through a device and causes localised heating - that's the underlying science, it's that simple. The large current flows when there's a large voltage across two or more pins, and that voltage comes from any electrostatic charge which exists.
An ESD-safe mat is dissipative, ie. slightly conductive, so although it will allow charge to leak away to earth, it does so slowly enough that any resulting currents which flow in a device will be small and harmless. In fact it doesn't even matter if the mat's earthed or not, provided it's at the same potential as the components and the operator (ie. you!)
A wooden or plastic mat is insulating, so charge remains on its surface which can result in harmful ESD events in a device. Plastic is the worst; most factories where electronic equipment is assembled won't even allow plastic objects (crisp packets, lunch boxes and similar) into the assembly area at all for this very reason.
On the other hand, a metal surface allows charge to flow too quickly (ie. large current) - which is exactly what you're trying to avoid in the first place. So not only is it arguably even worse from an ESD point of view, it'll also short out your project if you power it up on the bench. If you're working on live equipment then it's a safety hazard too.
My advice would be to treat yourself to a proper anti-static mat with an earthing plug and wrist strap. They're not expensive, are intended to resist solder splashes, and will protect your bench and your components from unfortunate mishaps.