- Mon Jan 10, 2011 10:49 pm
#117060
Hello All, I am new and was recommended to this website by faculty at my university. I have a BS in chemical engineering and am currently working on the undergrad pre-reqs for a masters in EE. I would love to build a forward viewing IR scope. From what I understand this site sells DSP/microcontrolers with multipule analouge inputs with built in LCD screens. Do you sell microbolo meters here? Do you sell optics/lenses or know where I could order them or the scope case or where I could have a shell made.
The reason I need 2 inputs is because I want to display an IR image as well as the visible light image (overlayed on each other), there will be some challenges on the sensing device side to figure out how im going to do that without having redundant optics. Since IR is very close to the visible spectrum I am hoping I can use traditional visible light optics to focus IR along with the visible light without any/much distortion in the IR zooming/focusing, then the challenge would be to duplicate the image for 2 different sensing devices. Can the DSP/microcontrolers be battery operated?
I can program in VB but it would not be a stretch for me to learn C or C++ if nessicary, but VB would be ideal. I am also eventually going to take a DSP class and possibly a VLSI class in the future as well as some optics classes.
Thank you for the help, I am looking forward to the parallel journey into a masters degree and doing some cool things with electronics.
The reason I need 2 inputs is because I want to display an IR image as well as the visible light image (overlayed on each other), there will be some challenges on the sensing device side to figure out how im going to do that without having redundant optics. Since IR is very close to the visible spectrum I am hoping I can use traditional visible light optics to focus IR along with the visible light without any/much distortion in the IR zooming/focusing, then the challenge would be to duplicate the image for 2 different sensing devices. Can the DSP/microcontrolers be battery operated?
I can program in VB but it would not be a stretch for me to learn C or C++ if nessicary, but VB would be ideal. I am also eventually going to take a DSP class and possibly a VLSI class in the future as well as some optics classes.
Thank you for the help, I am looking forward to the parallel journey into a masters degree and doing some cool things with electronics.